您好:
我正在使用高压电机控制套件tmdshvmtrpfckit,在用CCS v5将TI提供的控制算法模板送往控制板时,一直提示连接不通。
请问这种方式控制芯片时,电机控制板上的各个短路套以及芯片(28035)上的开关应该怎么设置?我目前的状态是将芯片上的SW2置为1-0(boot from SCI),并且将主板上的J9短路(使能JTAG),但是貌似不行。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我正在使用高压电机控制套件tmdshvmtrpfckit,在用CCS v5将TI提供的控制算法模板送往控制板时,一直提示连接不通。
请问这种方式控制芯片时,电机控制板上的各个短路套以及芯片(28035)上的开关应该怎么设置?我目前的状态是将芯片上的SW2置为1-0(boot from SCI),并且将主板上的J9短路(使能JTAG),但是貌似不行。
建议您安装一个ControlSuite,里面有详细的使用说明,实验介绍之类的文档。按照说明的要求,把Jumper都设置好!
按照使用说明,建立好CCS work space和工程。
http://www.ti.com/tool/controlsuite

建议楼主可以这样设置:
[Main]的J3, J4 , J5接上,然后用外接15V的适配器供电。
[Main]的J9:如果是使用CCS连接调试时将J9接上;如果是不接仿真器单片机模式时J9不接。
控制卡上的SW2接到1,1就好了。
控制卡上的SW1:如果是接仿真器时调试时就打到ON;如果是连串口通过GUI界面调试就打到OFF。