This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335CAN通信配置问题



各位大神好,CAN通信波特率500K,我遇到个CAN配置问题,希望得到帮助,问题描述如下:

1 原来我是30M的晶振,配置成主频率150M(30*10/2),485通信正常,CAN通信正常。CAN配置如:

#if (CPU_FRQ_150MHZ) // CPU_FRQ_150MHz is defined in DSP2833x_Examples.h
ECanaShadow.CANBTC.bit.BRPREG = 9;
ECanaShadow.CANBTC.bit.TSEG2REG = 2;
ECanaShadow.CANBTC.bit.TSEG1REG = 10;
#endif

SAM 设置成了1,SJW设置成了0.

2 现在我换成24M的晶振,配置成主频144M(24*6/1),依据144M的主频配置的485通信正常。但是CAN通信无法正常运行。现在CAN通信采用了DS301标准里面的推荐配置,详细如下:

#if (CPU_FRQ_144MHZ) // CPU_FRQ_144MHz is defined in DSP2833x_Examples.h
ECanaShadow.CANBTC.bit.BRPREG = 8;
ECanaShadow.CANBTC.bit.TSEG2REG = 1;
ECanaShadow.CANBTC.bit.TSEG1REG = 12;
#endif

SAM 设置成了1或者0都试过不行,SJW设置成了0.

希望大神们能帮我解决,谢谢!