This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335外扩ram



内部ram的空间感觉不够用,想将程序放在外部ram中运行,在进行外部ram实验时,发现了如下问题。ram是参考ezdsp的接口设计的,

ZONE7B     : origin = 0x20FC00, length = 0x004000;是外部ram的数据地址。

#pragma DATA_SECTION(DMABuf2,"ZONE7DATA");

volatile Uint16 DMABuf2[BUF_SIZE];

 DMABuf2是一个定义在外部ram以 0x20FC00为初始地址的数组;

for (i=0; i<BUF_SIZE; i++)//BUF_SIZE=1024;
{

DMABuf2[i] = i;
// x=DMABuf2[i] ;
}   该部分主要是实现对外部ram的写操作。

原理上我认为应该是得到DMABuf2[0]=0,DMABuf2[1]=1.........类推。

实际过程中DMABuf2[0]的值在不断变化,DMABuf2[1]=0;DMABuf2[2]=1;..........以此类推。

截图如下

请问是硬件还是软件的原因呢?