This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mcbsp的spi从模式



设计一个stm32和dsp28335之间的spi通信,想实现一个片选信号cs电平变化的过程传多次数据。即主机cs电平一直拉低,然后与从机一直传输数据,从机为dsp,采用接收中断的方式。但是发现cs电平的一次变化只能传一次数据。

总结一下就是在每次发送数据前都要对spi进行片选使能,为什么不能一次选中,之后进行多次的传输?

mcbsp配置

按照如图所示的配置:

McbspbRegs.SPCR1.bit.RINTM = 2;// 设置为cs低电平触发
McbspbRegs.MFFINT.bit.RINT = 1;//打开接受中断

  • 一次传输多个数据时,会出现rrdy位不置位的现象?这是为什么?

  • The SPISTE pin operates as the slave-select pin. An active-low signal on the SPISTE pin allows the slave
    SPI to transfer data to the serial data line; an inactive- high signal causes the slave SPI serial shift register
    to stop and its serial output pin to be put into the high-impedance state. This allows many slave devices to
    be tied together on the network, although only one slave device is selected at a time

    如果不把电平拉高,就一直发送数据。

    ERIC