你好,请问怎样设置才能使正在工作的某个PWM停下来?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主参考以下:
初始化配置:
EALLOW;
EPwm1Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
EPwm2Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
EPwm3Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
// What do we want the OST/CBC events to do?
// TZA events can force EPWMxA
// TZB events can force EPWMxB
EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWMxA will go low 根据需要设置停止输出时的PWM电平。
EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low
EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWMxA will go low
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low
EPwm3Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWMxA will go low
EPwm3Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low
EDIS;
以下为停止PWM输出:
// Stop PWM output
//===========================================================================
//Force trip EPwm1,2,3
//===========================================================================
EALLOW;
EPwm1Regs.TZFRC.bit.OST = 0x1; //disabPWMl
EPwm2Regs.TZFRC.bit.OST = 0x1; //disabPWM2
EPwm3Regs.TZFRC.bit.OST = 0x1; //disabPWM3
EDIS;
以下为使能PWM输出:
// Enable PWM output
//===========================================================================
//EnablePWM EPwm1,2,3
//===========================================================================
EALLOW;
EPwm1Regs.TZCLR.bit.OST = 1; //EnablePWM1
EPwm2Regs.TZCLR.bit.OST = 1; //EnablePWM2
EPwm3Regs.TZCLR.bit.OST = 1; //EnablePWM3
EDIS;
请问这个地方
EPwm1Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
EPwm2Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
EPwm3Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
是否是应该改成OSHT2 OSHT3。如果你这样设置道理是什么样子的?是否是只用1个OSHT1就可以完成6路pwm的封锁呢?
OSHT1为1代表允许TZ1 为OSHT保护模式,任何一个TZ信号都可以配置为保护一个或者多个PWM模块的PWM输出。因此下面的配置,可以实现6路PWM的封锁。
EPwm1Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
EPwm2Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT
EPwm3Regs.TZSEL.bit.OSHT1 = 1; //enable TZ1 for OSHT