This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一个关于ADC采样保持时钟(S/H时钟)的问题



我现在在做28335ADC模块的采样,使用的是软件触发,通过分频得到采样保持时钟,现在,我想请问一下,如何控制这个时钟的占空比,使采样的时候采样时钟正好出现在一个信号的中间位置,我看数据手册,怎么就是找不到相关的,难道信号一进来就开始采样吗?如果是正弦信号,采样得到的岂不是误差很大。怎么也搞不明白,希望望指教啊~

  • 您好,28335的ADC采用了SOC(start of conversion)的方式进行采样控制,即通过事件来触发采样(您采用的为软件触发的方式),同时增加了可编程的S/H时间,这段时间是为了使外部被采样量化信号能够充分的对采样电容充电,以便转换模块可以正确的读取输入信号的值,由于ADC使用的clock频率较高,因此这段S/H时间比较短,可以认为外部被采样信号基本维持不变。如果需要采样到信号的中间位置,需要您通过设置触发事件开始的位置来控制,并按照需要设置合适的S/H时间。

  • ”如果需要采样到信号的中间位置,需要您通过设置触发事件开始的位置来控制“.。这句话怎么理解,在哪个寄存器可以设置触发事件开始的位置呢?为什么在28335ADC的手册中找不到。希望得到您的帮助,谢谢!

  • ”如果需要采样到信号的中间位置,需要您通过设置触发事件开始的位置来控制“.。这句话怎么理解,在哪个寄存器可以设置触发事件开始的位置呢?为什么在28335ADC的手册中找不到。希望得到您的帮助,谢谢!

  • ADC 采样的开始,可以用下面三个触发源触发:

    – S/W - software immediate start

    – ePWM 1-6

    – GPIO XINT2

    那句话我的理解是说:如果你知道一个信号的周期,可以在想要采样的时间点去触发ADC采样。

    比如说50Hz的正弦,想在90度和270度的位置采样。

    首先你可以用比较器捕捉过零点,用外中断告诉C2000,然后用Timer计时,在5ms的位置软件触发采样。

  • 您想问的问题是如何确定触发采样时间吧,像Victor说的,提供了3种触发源,如何触发需要您自己去设置,根据您的信号特点,频率,幅值等等。