This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一个关于28335ADC采样的问题



我使用的是28335的ADC模块进行采样,使用的触发方式是软件触发,如何设置采样时钟周期,(即 每隔多长时间采一次),在数据手册上没有看到,请帮忙指点一下,谢谢!

  • 你可以使用延时嘛

  • 您好,28335的ADC采用了SOC(start of conversion)的方式进行采样控制,即通过事件来触发采样,您采用的为软件触发的方式,只有当您通过软件来触发采样时才发生一次采样;一次采样从开始到结束涉及了两个主要部分:采样保持时间和转换时间,每个时间段均包含了多个周期的ADCCLK;采样时钟ADCCLK的频率可以根据您的需要进行设置,最高的ADCCLK可以达到25MHz。具体这些参数如何设置需要根据您想要得到的采样率等指标来设定。