This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS6.0: Code Composer debug not working: the semaphore for the test bus controller is in a time-out state



我想将一个示例程序( ADC单通道)下载到我的ccs上面,,但是当我单击debug图标进行调试时,代码停止响应,然后最终返回错误:
The semaphore for the test bus controller is in a time-out state.
Unified-SCIF was unable to acquire the semaphore used to
express ownership of a controller by a utility or debugger.
You may have to exit other clients because the timeout occurred.

测试总线控制器的信号量处于超时状.。统一无法获取用于接收的信号量,通过应用工具或调试器来表示控制器的所有权。

您可能必须退出其他客户端,因为超时发生了。我在一台windows电脑上工作,我以为我的一切都是正确的,但是我很容易出错。有什么办法解决它吗?


谢谢