各位:
在安装完CCS6.1.3以及各个插件后,出现附件中无法识别280049M的情况~~有谁遇到相同情况,请帮忙解答下,如果配置成custom c2000就是OK的~~可以编译的~~系统是window xp sp3
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位:
在安装完CCS6.1.3以及各个插件后,出现附件中无法识别280049M的情况~~有谁遇到相同情况,请帮忙解答下,如果配置成custom c2000就是OK的~~可以编译的~~系统是window xp sp3
F28004x_DEV_USER_GUIDE中有讲到对ccs的要求
在C:\ti\c2000\C2000Ware_1_00_00_00\device_support\f28004x\docs中:
F28004x Example Projects
Code Composer Studio (CCS) Minimum Requirement: v6.2.0.00050 (Recommended: v7.0)
Example projects tested with: C2000 Compiler v16.9.1.LTS
zhenxing zhang2 说:为什么我都没申请到样片
您是否是按照链接中给出的步骤进行操作的呢:
http://www.ti.com.cn/general/cn/docs/gencontent.tsp?contentId=71114&keyMatch