程序中调用sprintf函数 报错:program will not fit into available memory ;(在线调试模式,使用官方提供RAM CMD文件)
这个函数应该占用内存资源相对较多,请问有什么办法可以有效解决这个问题?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
程序中调用sprintf函数 报错:program will not fit into available memory ;(在线调试模式,使用官方提供RAM CMD文件)
这个函数应该占用内存资源相对较多,请问有什么办法可以有效解决这个问题?谢谢。
参考下e2e的帖子
https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/266958?tisearch=e2e-sitesearch&keymatch=program%20will%20not%20fit%20into%20available%20memory
https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/540367?tisearch=e2e-sitesearch&keymatch=sprintf%20%20%20program%20will%20not%20fit%20into%20available%20memory
在map文件中“.text.1 0 00000000 00000c05 FAILED TO ALLOCATE”,问题应该是出在这里
CMD文件即为官方提供的:
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x000080, length = 0x000380
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x00007E /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
ramfuncs : > RAMM0 PAGE = 0
.text : >>RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4, PAGE = 0
.cinit : > RAMM0, PAGE = 0
.pinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
.ebss : > RAMLS5, PAGE = 1
.econst : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}
请问应该如何调整?