This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28335内部FLASH擦除失败



1、DSP28335正常工作一段时间,某天突然出现烧写内部FLASH过程中,FLASH擦除失败,报错信息为:

Flash Programmer :Error  srasing Flash Memory.

Trouble writing Memory Block at 0x33a000 on page 0 of length 0x289

2、通过RAM运行flash_api code, 执行擦除操作时,返回值是24(0x18),根据手册 返回值24表示 STATUS_FAIL_PRECOMPACT

Erase operation failed because the pre- compaction portion failed.

The pre-compaction is applied to all sectors on the device.

The FLASH_ST structure will return a fail address corresponding to the first sector fails this step

3、通过RAM运行flash_api code,执行写入操作时,能够在FLASH为全F的区域成功写入,并能够读取,写入后由于不能擦除,无法再次写入。

4、尝试了在ONCHIP TOOL 内部使用DEPLTION RECOVERY,指令无效,返回超时,同时在程序内添加depRecovery ()函数,返回23(STATUS_FAIL_COMPACT)

请问这是什么原因造成的?有什么合适的方法能够解决该问题?

谢谢