This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377上CLA协处理器可以直接通过EMIF写数据到外部FPGA吗?

28377上CLA协处理器可以直接通过EMIF写数据到外部FPGA吗?有没有其它方法可以实现?

  • CLA 访问不了EMIF。

    可以通过CPU作为中介进行通信。

    ERIC

  • 为了能够实时将CLA协处理器计算的数据发送到FPGA,是否可以由CLA协处理器内软件触发一次CPU的高级中断,如ADCA1中断;我尝试了在CLA协处理器结尾用GPIO管脚触发EINT1,只是从协处理器结尾到进入EINT1中断函数大约需要耗时300ns,如果可行,应该还是要尽量通过软件使能中断实现吧,请赐教!

  • 您好,请问28377的EMIF接口用的是同步还是异步模式和FPGA通讯?我看EMIF的同步模式只支持SDRAM,而FPGA内部RAM又是同步的,不知道该怎么连接二者,恳请楼主指教。
  • 您好,请问28377的EMIF接口用的是同步还是异步模式和FPGA通讯?我看EMIF的同步模式只支持SDRAM,而FPGA内部只有通同步双口SRAM,不知道该怎么连接二者,恳请楼主指教。