This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

初学者关于28335开发的疑问



列成点说吧:

1)我是用CCS3.3的,感觉一个新的过程需要添加很多文件,做许多设置。我现在的仿真器只支持到4.1,请问ccs4.1的新建工程要比3.3的如意么?

2)我自己建立了一个串口的工程,编译通过,但是加载到DSP后没有成功和电脑通讯,但是同样的源程序在模板工程里编译就可以正常运行,这种情况一般是什么原因?

3)接着3说,可以把旧的工程复制后,在里面重新写新的源程序么?

4)库文件需要自己手动添加么?我看到很多工程的library文件夹都是空的,但是也调用了库,如何理解?

5}我看驱动库的头文件里面,05年版本的有函数申明,10年版本的就只有宏定义了,哪一种好?

先就这些吧,希望大虾能答疑解惑,感激不尽。