Other Parts Discussed in Thread: AFE031
我看了Hardware Platform
v5.2.1.0: F28069 + AFE031
和芯片资源需求
F28069 build (Cenelec A)
AppBoot Flash Sector A
DFU Flash Sector H
G3 image FLASH (Sector B-G): 176/192 kB
RAM: 87/96 kB
Peak MIPs 88 MIPs
是不是说,作为一个终端设备,比如说光伏逆变器产品,那么我的控制器没剩下多少FLASH和RAM给我用了?就剩下16K的FLASH和6K的RAM给我做控制系统用了?可以这样说吗?