This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:F28335编译错误 placement fails for object "csmpasswds"

采用CCS3.3进行编译,cmd文件为例程文件,链接时出现error:placement fails for object “csmpasswds”

  • Error: placement fails for object "csmpasswds"

    This is an issue in an early version of the 5.x compiler/linker. The linker is complaining about a section with the same name on page 0 and page 1. You can change the name of one of these sections in the liker .cmd file. The suggested fix, however, is to update the codegen tools.
    你好,看下cmd文件中的page 0 and page 1有same name,更改其中一个即可。