This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28035高精度HRPWM发波



各路大神:

        请教个问题F28035有7对14路PWM波,其中有7路高精度PWM为每一对的A路,我在做实验的时候用的HRPWM波功能,AB两路输出用的都是A路的波源也就说AB两路都是选择的A路的AQ动作,死区为零即EPwm1Regs.DBCTL.bit.IN_MODE = 0x00;EPwm1Regs.DBCTL.bit.POLSEL =0x00;EPwm1Regs.DBCTL.bit.OUT_MODE = 0x03;EPwm1Regs.DBFED =0;EPwm1Regs.DBRED = 0;在改变EPwm1Regs.CMPA.half.CMPAHR的值时,示波器测A路的PWM波占空比即边沿发生改变,B路的PWM波占空比保持不变,请问HRPWM波的边沿发生作用的时候是在AQ动作时还是在最终引脚输出时,如果说是在AQ执行动作时那么就和实验结果相悖,如果在最终输出时那是在AQ之后哪一个模块起作用的,谢谢!