dsp2808和2812的主要区别有那些?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
F2812有扩展的数据总线和地址总线,2808没有
F2812内部的FLASH大
2808的外设比2812多
TMS320F28335与TMS320F2812的区别
TMS320F28335数字信号处理器是TI公司最新推出的32位浮点DSP控制器。与TMS320F2812定点DSP相比, TMS320F28335增加了单精度浮点运算单元(FPU) 和高精度PWM,且Flash增加了一倍(256K×16Bit) , 同時增加了DMA功能, 可将ADC转换结果直接存入DSP的任一存储空间。此外, 它还增加了CAN通讯模块、SCI接口和SPI接口。
TMS320F28355的主频最高为150MHz, 同时具有外部存储扩展接口、看门狗、三个定时器、18个PWM输出和16通道的12位AD转换器。
TMS320F28335与TMS320F2808的区别
F2808目前主要应用于电机控制用电力电子变流器中。从某种意义上说,F28335是F2808的升级版本,两者的核心结构和外设配置都十分相近。但是,除了上述的共同优势外,F28335克服了F2808的一个最致命的弱点,即外设扩展性弱。
F28335拥有类似2812的XINTF(External Interface外部接口),但其功能更为强大,是16/32位数据位宽可配置,DMA可控制的。在系统设计时,可以通过该接口很方便地扩展片外存储器和其他外设,独立设置它们的控制时序,这对于现在电力电子变流装置的控制十分重要。因为片上外设往往并不能满足系统全部的控制要求,这就需要系统具有良好的可扩展性。F28335的可扩展性相比F2808上了一个台阶。