This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

warning #10247-D: creating output section "MYSEC" without a SECTIONS specification

Other Parts Discussed in Thread: F28M36P63C2, SYSBIOS

使用的CCS版本Code Composer Studio 6.0.1; 使用的芯片F28M36

使用tirtos_c2000_2_00_01_23,xdctools_3_30_03_47_core

以下为cmd文件,我新建了一个空的c2000的RTOS工程,在默认cmd文件最后一行增加了MYSEC,在main文件我定义了#pragma DATA_SECTION(DMABuf1,"MYSEC");编译的时候总是报warning #10247-D: creating output section "MYSEC" without a SECTIONS specification

在m3核,我也建了同样的工程,也在cmd和main文件做了同样的操作,编译没有warning,在线求解,谢谢

 *  ======== F28M36P63C2.cmd ========
 *  Define the memory block start/length for the F28M36P63C2 C28
 */

MEMORY
{
PAGE 0:    /* Program Memory */

    FLASH       : origin = 0x100000, length = 0x3FF80
    BEGIN       : origin = 0x13FFF0, length = 0x2
   
PAGE 1 :   /* Data Memory */
  
    M01SARAM    : origin = 0x0,      length = 0x800     /* on-chip RAM block M0, M1 */
    PIEVECT     : origin = 0xD00,    length = 0x100
    L03SARAM    : origin = 0x8000,   length = 0x4000    /* on-chip RAM block L0-L3 */
    S07SHRAM    : origin = 0xC000,   length = 0x8000
    CTOMMSGRAM  : origin = 0x3F800,  length = 0x400
    MTOCMSGRAM  : origin = 0x3FC00,  length = 0x400
}

SECTIONS
{
    /* Allocate program areas: */
    .text       : > FLASH   PAGE = 0
    .cinit      : > FLASH   PAGE = 0
    .pinit      : > FLASH   PAGE = 0
    .binit      : > FLASH   PAGE = 0
    ramfuncs    : LOAD = FLASH      PAGE = 0,
                  RUN  = L03SARAM   PAGE = 1,
                  LOAD_START(_RamfuncsLoadStart),
                  LOAD_SIZE(_RamfuncsLoadSize),
                  LOAD_END(_RamfuncsLoadEnd),
                  RUN_START(_RamfuncsRunStart)

    /* Initalized sections go in Flash */
    .econst     : > FLASH   PAGE = 0
    .switch     : > FLASH   PAGE = 0

    /* Allocate uninitalized data sections: */
    .stack      : > M01SARAM | L03SARAM PAGE = 1
    .ebss       : > M01SARAM | L03SARAM PAGE = 1
    .esysmem    : > L03SARAM | M01SARAM PAGE = 1
    .cio        : > L03SARAM | M01SARAM PAGE = 1
    .args       : > L03SARAM | M01SARAM PAGE = 1

    .MYSEC  :>L03SARAM PAGE = 1
}

以下为main文件开头部分

#include <xdc/std.h>

#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <xdc/cfg/global.h>

#include <ti/sysbios/BIOS.h>

#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Event.h>
#include <ti/sysbios/knl/Semaphore.h>

#include <ti/sysbios/family/c28/Hwi.h>
#include "F28M36x_Device.h"     // F28M36x Headerfile Include File
#include "F28M36x_GlobalPrototypes.h"         // Prototypes for global functions
                                              // within the .c files.
#include <string.h>

#pragma DATA_SECTION(DMABuf1,"MYSEC");

。。。。。

 

 

 

  • 我把我的main函数全都贴出来给大家看看,我需要用DMA,本想在定义2个DMARAML2,DMARAML3定义DMA的源和目标数组,但总是报 without a SECTIONS specification的错误,于是我就把工程里其它文件都删了,新建了一个工程,用系统默认的cmd,在L03SARAM增加MYSEC,也报同样的错误,实在想不通了

     *  ======== main.c ========
     */

    #include <xdc/std.h>

    #include <xdc/runtime/Error.h>
    #include <xdc/runtime/System.h>
    #include <xdc/cfg/global.h>

    #include <ti/sysbios/BIOS.h>

    #include <ti/sysbios/knl/Task.h>
    #include <ti/sysbios/knl/Event.h>
    #include <ti/sysbios/knl/Semaphore.h>

    #include <ti/sysbios/family/c28/Hwi.h>
    #include "F28M36x_Device.h"     // F28M36x Headerfile Include File
    #include "F28M36x_GlobalPrototypes.h"         // Prototypes for global functions
                                                  // within the .c files.
    #include <string.h>

    #pragma DATA_SECTION(DMABuf1,"MYSEC");
    //#pragma DATA_SECTION(DMABuf2,"MYSEC");

    // Buffer size
    #define BUF_SIZE    10
    #define AD_BUF_LEN  10


    // Prototype statements for functions found within this file.
    void local_DINTCH1_ISR(UArg arg);
    ti_sysbios_family_c28_Hwi_Struct dmach1hwi;

    Uint16 ADC_Buf[8];
    Uint32 CH1_Buf[10];
    Uint32 CH3_Buf[10];
    Uint32 g_ulDataCH1;
    Uint32 g_ulDataCH2;
    Uint32 g_ulDataCH3;
    Uint32 g_ulDataCH4;
    Uint16 pCnt;
    Uint16 src_test[10];
    volatile Uint16 DMABuf1[10];
    volatile Uint16 DMABuf2[10];
    volatile Uint16 *DMADest;
    volatile Uint16 *DMASource;
    volatile Uint32 transfer_count;

    //---------------------------------------------------------------------------
    // InitGpio:
    //---------------------------------------------------------------------------
    // This function initializes the Gpio to a known (default) state.
    // For more details on configuring GPIO's as peripheral functions,
    // refer to the individual peripheral examples and/or GPIO setup example.
    void InitGpio(void)
    {
        EALLOW;

        // Each GPIO pin can be:
        // a) a GPIO input/output
        // b) peripheral function 1
        // c) peripheral function 2
        // d) peripheral function 3
        // By default, all are GPIO Inputs
        GpioG1CtrlRegs.GPAMUX1.all = 0x0000;    // GPIO functionality GPIO0-GPIO15
        GpioG1CtrlRegs.GPAMUX2.all = 0x0000;    // GPIO functionality GPIO16-GPIO31
        GpioG1CtrlRegs.GPBMUX1.all = 0x0000;    // GPIO functionality GPIO32-GPIO44
        GpioG1CtrlRegs.GPBMUX2.all = 0x0000;    // GPIO functionality GPIO45-GPIO63
        GpioG1CtrlRegs.GPCMUX1.all = 0x0000;    // GPIO functionality GPIO64-GPIO79
        GpioG1CtrlRegs.GPCMUX2.all = 0x0000;    // GPIO functionality GPIO80-GPIO95
        GpioG1CtrlRegs.GPDMUX1.all = 0x0000;    // GPIO functionality GPIO96-GPIO111
        GpioG1CtrlRegs.GPDMUX2.all = 0x0000;    // GPIO functionality GPIO112-GPIO127
        GpioG1CtrlRegs.GPEMUX1.all = 0x0000;    // GPIO functionality GPIO128-GPIO135

        GpioG2CtrlRegs.GPGMUX1.all = 0x0000;    // GPIO functionality GPIO192-199
        GpioG2CtrlRegs.AIOMUX1.all = 0x0000;    // Dig.IO funct. applies to
                                                // AIO2,4,6,10,12,14
        GpioG2CtrlRegs.AIOMUX2.all = 0x0000;    // Dig.IO funct. applies to
                                                // AIO18,20,22,26,28,30

        GpioG1CtrlRegs.GPADIR.all = 0x0000;     // GPIO0-GPIO31 are inputs
        GpioG1CtrlRegs.GPBDIR.all = 0x0000;     // GPIO32-GPIO63 are inputs
        GpioG1CtrlRegs.GPCDIR.all = 0x0000;     // GPIO64-GPIO95 are inputs
        GpioG1CtrlRegs.GPDDIR.all = 0x0000;     // GPIO96-GPIO127 are inputs
        GpioG1CtrlRegs.GPEDIR.all = 0x0000;     // GPIO128-GPIO159 are inputs
        GpioG2CtrlRegs.GPGDIR.all = 0x0000;     // GPIO192-199 are inputs
        GpioG2CtrlRegs.AIODIR.all = 0x0000;     //
                                                //
                                                // AIO2,4,6,19,12,14,18,20,22,26,28,30
                                                // are digital inputs

        // Each input can have different qualification
        // a) input synchronized to SYSCLKOUT
        // b) input qualified by a sampling window
        // c) input sent asynchronously (valid for peripheral inputs only)
        GpioG1CtrlRegs.GPAQSEL1.all = 0x0000;   // GPIO0-GPIO15 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPAQSEL2.all = 0x0000;   // GPIO16-GPIO31 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPBQSEL1.all = 0x0000;   // GPIO32-GPIO44 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPBQSEL2.all = 0x0000;   // GPIO45-GPIO63 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPCQSEL1.all = 0x0000;   // GPIO64-GPIO79 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPCQSEL2.all = 0x0000;   // GPIO80-GPIO95 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPDQSEL1.all = 0x0000;   // GPIO96-GPIO111 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPDQSEL2.all = 0x0000;   // GPIO112-GPIO127 Synch to SYSCLKOUT
        GpioG1CtrlRegs.GPEQSEL1.all = 0x0000;   // GPIO128-GPIO135 Synch to SYSCLKOUT
        GpioG2CtrlRegs.GPGQSEL1.all = 0x0000;   // GPIO192-GPIO199 Synch to SYSCLKOUT

    // Enable internal pull-up for the selected pins

    // Pull-up enable should be set in the
    // GPIO_O_PUR register in the M3 code.

        EDIS;
    }


    void init_sys(void)
    {

     // Step 1. Initialize System Control:
     // PLL, WatchDog, enable Peripheral Clocks
     // This example function is found in the F28M36x_SysCtrl.c file.
         InitSysCtrl();

     // Copy time critical code and Flash setup code to RAM
     // This includes the following functions:  InitFlash();
     // The  RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart
     // symbols are created by the linker. Refer to the device .cmd file.
    //      memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);

     // Call Flash Initialization to setup flash waitstates
     // This function must reside in RAM
    //     InitFlash();

     // Initialize the PIE control registers to their default state.
     // The default state is all PIE interrupts disabled and flags
        // are cleared.
     // This function is found in the F28M36x_PieCtrl.c file.
     //    InitPieCtrl();

     // Disable CPU interrupts and clear all CPU interrupt flags:
         /*IER = 0x0000;
         IFR = 0x0000;*/

     // Initialize the PIE vector table with pointers to the shell Interrupt
     // Service Routines (ISR).
     // This will populate the entire table, even if the interrupt
     // is not used in this example.  This is useful for debug purposes.
     // The shell ISR routines are found in F28M36x_DefaultIsr.c.
     // This function is found in F28M36x_PieVect.c.
         //InitPieVectTable();

     // Enable global Interrupts and higher priority real-time debug events:
         EINT;  // Enable Global interrupt INTM
         ERTM;  // Enable Global realtime interrupt DBGM
     // Initialize GPIO:
         InitGpio();//set the GPIO to it's default state.
      /* Explicit posting of Event_Id_00 by calling Event_post() */

    }

    void ConfigEpwm1( void )
    {
        // Assumes ePWM1 clock is already enabled in InitSysCtrl();
        EALLOW;
        // Enable SOCA and SOCB
        EPwm1Regs.ETSEL.bit.SOCAEN         = 1;      // Enable SOC on A group
        EPwm1Regs.ETSEL.bit.SOCASEL        = 0x4;    // Select SOC from CMPA/CMPC on up count
        EPwm1Regs.ETSEL.bit.SOCASELCMP     = 0x1;    // CMPC

        EPwm1Regs.ETPS.bit.SOCAPRD         = 3;      // Generate SOCA pulse on every 3rd event

        // Time-base registers
        EPwm1Regs.TBPRD = 14999;                    // Set EPWM timer period
        EPwm1Regs.TBPHS.all = 0;                     // Time-Base Phase Register
        EPwm1Regs.TBCTR = 0;                         // Time-Base Counter Register
        EPwm1Regs.TBCTL.bit.PRDLD = 1;    // Set Immediate load
        EPwm1Regs.TBCTL.bit.CTRMODE = 0;   // Count-up mode: used for asymmetric PWM

        EPwm1Regs.TBCTL.bit.PHSEN = 0;      // Disable phase loading
        EPwm1Regs.TBCTL.bit.SYNCOSEL = 3;

        // Set TBCLK frequency
        EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0;     // TBCLK = SYSCLKOUT
        EPwm1Regs.TBCTL.bit.CLKDIV = 0;

        // Setup shadow register load on ZERO
        EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0;
        EPwm1Regs.CMPCTL.bit.LOADAMODE = 0; // load on CTR=Zero

        // Set Compare values
        EPwm1Regs.CMPC = 500;
        EDIS;
    }

    void StartDMACH1(void)
    {
        EALLOW;
        DmaRegs.CH1.CONTROL.bit.RUN = 1;
        EDIS;
    }

    /*
     *  ======== taskFxn ========
     */
    Uint16 j=0,state=0;
    Void taskFxn(UArg a0, UArg a1)
    {
     Int16 i;
     Hwi_Params             hwiParams;

     System_printf("enter taskFxn()\n");

        init_sys();

        pCnt = 0;
     g_ulDataCH1 = 0;
     g_ulDataCH2 = 0;
     g_ulDataCH3 = 0;
     g_ulDataCH4 = 0;
     for(i=7;i>=0;i--) // 清帧缓冲区
     {
      ADC_Buf[i] = 0;
     }
     for(i = 0; i < 10; i++)
     {
      src_test[i] = i+1;
     }

     for(i=AD_BUF_LEN-1;i>=0;i--)//清缓冲区
     {
      CH1_Buf[i] = 0;

      CH3_Buf[i] = 0;

     }

     EALLOW;
     Hwi_Params_init(&(hwiParams));
     Hwi_construct(&dmach1hwi, 80, local_DINTCH1_ISR,
            &(hwiParams), NULL);
     EDIS;

     // Initialize the DMA
     EALLOW;
     // Set up SOURCE address:
     DmaRegs.CH1.SRC_BEG_ADDR_SHADOW = (Uint32)(&src_test);//(&McbspaRegs.DRR2.all); // Point to beginning of source buffer
     DmaRegs.CH1.SRC_ADDR_SHADOW =     (Uint32)(&src_test);//(&McbspaRegs.DRR2.all);

     // Set up DESTINATION address:
     DmaRegs.CH1.DST_BEG_ADDR_SHADOW = (Uint32) &ADC_Buf[0];
     DmaRegs.CH1.DST_ADDR_SHADOW = (Uint32) &ADC_Buf[0];

     // Set up BURST registers:
     DmaRegs.CH1.BURST_SIZE.all = 0;  //0  1 word per burst
     DmaRegs.CH1.SRC_BURST_STEP = 0;  //0  Not used when bust size is 1 word
     DmaRegs.CH1.DST_BURST_STEP = 0;  //0  Not used when burst size is 1 word

     // Set up TRANSFER registers:
     DmaRegs.CH1.TRANSFER_SIZE = 5;     //   1024 burst per transfer
     DmaRegs.CH1.SRC_TRANSFER_STEP =0;//0xFFFF; //0  Don't change source addres between burst
     DmaRegs.CH1.DST_TRANSFER_STEP = 1; //  Destination address increment by 1 between burst
     // Set up WRAP registers:
     DmaRegs.CH1.SRC_WRAP_SIZE = 0xFFFF; // Put to maximum - don't want source wrap
     DmaRegs.CH1.SRC_WRAP_STEP = 0;  // Not used for wrap disabled
     DmaRegs.CH1.DST_WRAP_SIZE = 0xFFFF; // Put to maximum - don't want destination wrap
     DmaRegs.CH1.DST_WRAP_STEP = 0;  // Not used for wrap disabled
     // Set up MODE Register:
     DmaRegs.CH1.MODE.bit.PERINTSEL = 18;//epwm  //11;//timer0 // 15 McBSPA receive interrupt as channel trigger
     DmaRegs.CH1.MODE.bit.PERINTE = 1;       // Enable channel triggered by peripheral interrupt
     DmaRegs.CH1.MODE.bit.ONESHOT = 0;       // Disable one shot mode
     DmaRegs.CH1.MODE.bit.CONTINUOUS = 0;    // Enable continous run mode
     DmaRegs.CH1.MODE.bit.OVRINTE = 0;       // disable the overflow interrupt
     DmaRegs.CH1.MODE.bit.DATASIZE = 0;      // 16-bit data size transfers,1-32bit
     DmaRegs.CH1.MODE.bit.CHINTMODE = 1;// 0;  //0  Generate interrupt to CPU at beginning of transfer
     DmaRegs.CH1.MODE.bit.CHINTE = 1;        // Channel Interrupt to CPU enable

     // Clear any spurious flags:
     DmaRegs.CH1.CONTROL.bit.PERINTCLR = 1;    // Clear any spurious interrupt flags
     //DmaRegs.CH1.CONTROL.bit.SYNCCLR = 1;      // Clear any spurious sync flags
     DmaRegs.CH1.CONTROL.bit.ERRCLR = 1;        // Clear any spurious sync error flags

     DmaRegs.CH1.CONTROL.bit.RUN = 1;

     EDIS;

     ConfigEpwm1();

     // Step 5. Start the DMA
     transfer_count = 0;

    }

    /*
     *  ======== main ========
     */
    Int main()
    {
     Task_Handle task;
     Error_Block eb;

     System_printf("enter main()\n");

     Error_init(&eb);
     task = Task_create(taskFxn, NULL, &eb);
     if (task == NULL) {
      System_printf("Task_create() failed!\n");
      BIOS_exit(0);
     }

     BIOS_start();    /* does not return */
     return(0);
    }


    void local_DINTCH1_ISR(UArg arg)
    {
     register Uint32 DataTemp;
     Uint16 i;

     DataTemp = ADC_Buf[0];
     DataTemp <<= 16;
     DataTemp |= ADC_Buf[1];
     g_ulDataCH1 = DataTemp;

     DataTemp = ADC_Buf[2];
     DataTemp <<= 16;
     DataTemp |= ADC_Buf[3];
     g_ulDataCH2 = DataTemp;

     DataTemp = ADC_Buf[4];
     DataTemp <<= 16;
     DataTemp |= ADC_Buf[5];
     g_ulDataCH3 = DataTemp;


     DataTemp = ADC_Buf[6];
     DataTemp <<= 16;
     DataTemp |= ADC_Buf[7];
     g_ulDataCH4 = DataTemp;

     CH1_Buf[pCnt] = g_ulDataCH1;
     CH3_Buf[pCnt] = g_ulDataCH2;

     for(i = 0; i < 10; i++)
     {
      src_test[i] = src_test[i]+1;
     }

     if(pCnt<AD_BUF_LEN-1)
     {
      pCnt++;
     }
     else
     {
      pCnt = 0;
     }

     transfer_count++;
     PieCtrlRegs.PIEACK.all = PIEACK_GROUP7;
     StartDMACH1();

    }


     

  • 我知道问题在哪了,cmd文件里写的是.MYSEC,但#pragma DATA_SECTION(DMABuf1,"MYSEC");写的是MYSEC,少了一个.

    真是大意啊,折腾了好久

  • .MYSEC  :> L03SARAM PAGE = 1

    #pragma DATA_SECTION(DMABuf1,".MYSEC");

    以为是编译器的原因呢,这个.在大写前太小啦,不容易发觉。

  • 继续问一个问题,我想把编码器EQEP的位置信息通过DMA搬到指定区域,定时产生中断,但是手册里写的DMA Block Diagram里的C28x PERIPHERALS不包括EQEP,ram空间也只能用L2/L3,我可以修改cmd文件把EQEP改到RAML3空间里吗?

    F28M36x_Headers_BIOS.cmd里这样修改(红色部分)

    MEMORY
    {
     PAGE 0:    /* Program Memory */

     PAGE 1:    /* Data Memory */

       DEV_EMU             : origin = 0x000880, length = 0x000180     /* device emulation registers */
       CSM                 : origin = 0x000AE0, length = 0x000020     /* code security module registers */

       ADC1_RESULT         : origin = 0x000B00, length = 0x000020     /* ADC1 Results register */
       ADC2_RESULT         : origin = 0x000B40, length = 0x000020     /* ADC2 Results register */

       CPU_TIMER0          : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */
       CPU_TIMER1          : origin = 0x000C08, length = 0x000008     /* CPU Timer1 registers (CPU Timer1 & Timer2 reserved TI use)*/
       CPU_TIMER2          : origin = 0x000C10, length = 0x000008     /* CPU Timer2 registers (CPU Timer1 & Timer2 reserved TI use)*/

       PIE_CTRL            : origin = 0x000CE0, length = 0x000020     /* PIE control registers */

       DMA                 : origin = 0x001000, length = 0x000200     /* DMA registers */
      
       ASYSCTRLCONFIG      : origin = 0x001700, length = 0x000080     /* Analog System Control Configuration Registers */
            
       FLASH_REGS          : origin = 0x004000, length = 0x000300     /* Flash Control registers */
       FLASH_ECC           : origin = 0x004300, length = 0x000040     /* Flash/OTP ECC Error Log registers */
      
       M3PLL               : origin = 0x004400, length = 0x000010       /* M3 Clock Configuration Registers  */

       EPI_REGS            : origin = 0x004430, length = 0x000010       /* EPI Registers  */
      
       RAM_REGS            : origin = 0x004900, length = 0x000080     /* RAM Control registers */
       RAM_ERR_REGS        : origin = 0x004A00, length = 0x000080     /* RAM ECC/PARITY/ACCESS Error Log Registers */

       CM_MC_IPC           : origin = 0x004E00, length = 0x000040     /* C28 Control to Master IPC registers */  
         
       MCBSPA              : origin = 0x005000, length = 0x000040     /* McBSP-A registers */

       EPWM1               : origin = 0x005100, length = 0x000080     /* EPWM1 + HRPWM registers */
       EPWM2               : origin = 0x005180, length = 0x000080     /* EPWM2 + HRPWM registers */
       EPWM3               : origin = 0x005200, length = 0x000080     /* EPWM3 + HRPWM registers */
       EPWM4               : origin = 0x005280, length = 0x000080     /* EPWM4 + HRPWM registers */
       EPWM5               : origin = 0x005300, length = 0x000080     /* EPWM5 + HRPWM registers */
       EPWM6               : origin = 0x005380, length = 0x000080     /* EPWM6 + HRPWM registers */
       EPWM7               : origin = 0x005400, length = 0x000080     /* EPWM7 + HRPWM registers */
       EPWM8               : origin = 0x005480, length = 0x000080     /* EPWM8 + HRPWM registers */
       EPWM9               : origin = 0x005500, length = 0x000080     /* EPWM9 registers  (no HRPWM) */
       EPWM10              : origin = 0x005580, length = 0x000080     /* EPWM10 registers (no HRPWM) */
       EPWM11              : origin = 0x005600, length = 0x000080     /* EPWM11 registers (no HRPWM) */
       EPWM12              : origin = 0x005680, length = 0x000080     /* EPWM12 registers (no HRPWM) */

       ECAP1               : origin = 0x005A00, length = 0x000020     /* Enhanced Capture 1 registers */
       ECAP2               : origin = 0x005A20, length = 0x000020     /* Enhanced Capture 2 registers */
       ECAP3               : origin = 0x005A40, length = 0x000020     /* Enhanced Capture 3 registers */
       ECAP4               : origin = 0x005A60, length = 0x000020     /* Enhanced Capture 4 registers */
       ECAP5               : origin = 0x005A80, length = 0x000020     /* Enhanced Capture 5 registers */
       ECAP6               : origin = 0x005AA0, length = 0x000020     /* Enhanced Capture 6 registers */

       //EQEP1               : origin = 0x005B00, length = 0x000040     /* Enhanced QEP 1 registers */
       //EQEP2               : origin = 0x005B40, length = 0x000040     /* Enhanced QEP 2 registers */
       //EQEP3               : origin = 0x005B80, length = 0x000040     /* Enhanced QEP 3 registers */
       EQEP1               : origin = 0x00B000, length = 0x000040     /* Enhanced QEP 1 registers */
       EQEP2               : origin = 0x00B040, length = 0x000040     /* Enhanced QEP 2 registers */
       EQEP3               : origin = 0x00B080, length = 0x000040     /* Enhanced QEP 3 registers */

    。。。。。。。。

     *  ======== F28M36P63C2.cmd ========
     *  Define the memory block start/length for the F28M36P63C2 C28
     */

    MEMORY
    {
    PAGE 0:    /* Program Memory */

        FLASH       : origin = 0x100000, length = 0x3FF80
        BEGIN       : origin = 0x13FFF0, length = 0x2
       
    PAGE 1 :   /* Data Memory */
      
        M01SARAM    : origin = 0x0,      length = 0x800     /* on-chip RAM block M0, M1 */
        PIEVECT     : origin = 0xD00,    length = 0x100
        //L03SARAM    : origin = 0x8000,   length = 0x4000    /* on-chip RAM block L0-L3 */
        RAML01 :origin = 0x8000,   length = 0x2000
        RAML2 :origin = 0xA000,   length = 0x1000
        RAML3 :origin = 0xB000,   length = 0x1000
        S07SHRAM    : origin = 0xC000,   length = 0x8000
        CTOMMSGRAM  : origin = 0x3F800,  length = 0x400
        MTOCMSGRAM  : origin = 0x3FC00,  length = 0x400
    }

  • 我按照上面修改编译了一下,报了以下错我,求指点

    <Linking>
    "F:/PUMP/MCU/linear/F28M36x/MCU_C28_TEST/../cmd/c28/F28M36x_Headers_BIOS.cmd", line 80: error #10264:
       EQEP1 memory range overlaps existing memory range RAML3
    "F:/PUMP/MCU/linear/F28M36x/MCU_C28_TEST/../cmd/c28/F28M36x_Headers_BIOS.cmd", line 81: error #10264:
       EQEP2 memory range overlaps existing memory range RAML3
    "F:/PUMP/MCU/linear/F28M36x/MCU_C28_TEST/../cmd/c28/F28M36x_Headers_BIOS.cmd", line 82: error #10264:
       EQEP3 memory range overlaps existing memory range RAML3

  • 看了datasheet, EQEP的区间不能改