This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在使用用28335,CLKIN接外部时钟源(19.2Mhz有源晶振),X1接地,X2悬空。
焊了3快板,仿真器连接测试都通过,但只有1块板可以进入debug,另外2块提示CPU处于low power状态。
load程序后执行SysCtrlRegs.PLLSTS.bit.MCLKOFF = 1;语句也会提示CPU处于low power状态,与仿真器的连接断开。
如果跳过SysCtrlRegs.PLLSTS.bit.MCLKOFF = 1;语句,通过IO反转测试
while(1)
{
GpioDataRegs.GPCSET.bit.GPIO84 = 1;
GpioDataRegs.GPCCLEAR.bit.GPIO84 = 1;
}
GPIO高电平时间持续2us。
请帮助解决