This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035 CPU中断与CLA中断 冲突?

Other Parts Discussed in Thread: TMS320F28035

大家好!我现在用TMS320F28035做一个电源的控制,其中CLA处理闭环程序,由ADC触发,ADC采样由EPWM触发,这些调试中都没问题。现在想加一个Timer0的1kHz中断用来做定时,但是调试中发现使能PieCtrlRegs.PIEIER1.bit.INTx7 = 1之后(下面程序中标***部分),程序一运行就停止,且显示“No source available for "0x3ff599" ”,再运行还是马上停止显示同样的内容,我查了一下0x3ff599是属于Boot ROM。如果把使能中断那一行屏蔽掉,则运行正常(不产生Timer0中断)。我试过其他的中断,比如让CPU处理一个ADC中断,也会发生同样的问题。请问这是什么原因呢?

main()的内容为:

DeviceInit(); // Device Life support & GPIO

memcpy((Uint16 *)&RamfuncsRunStart,(Uint16 *)&RamfuncsLoadStart, (unsigned long)&RamfuncsLoadSize);

InitFlash();

CLA_Init();

InitEPwmGpio();

InitCpuTimers();

ConfigCpuTimer(&CpuTimer0, 60, 50000);

CpuTimer0Regs.PRD.all = mSec0_5; 

EPWM_CNF();

DPL_CLAInit(); // Digital Power (DP) library initialization

// INTERRUPT & ISR INITIALISATION

PieVectTable.TINT0 = &TimerIsr0; // 1 KHz ISR from CPU Timer 2

PieVectTable.EPWM1_TZINT = &EpwmTZ1;

EALLOW;

PieCtrlRegs.PIEIER1.bit.INTx7 = 1; // PIE level enable, Grp1 / Int7 TINT0*******************

PieCtrlRegs.PIEIER2.bit.INTx1 = 1; // PIE level enable, Grp2 / Int1 EPWM1_TZINT

EDIS;

IER |= M_INT1|M_INT2; // Enable CPU INT1&2 connected to EPWM1-6 INTs:

EINT; // Enable Global interrupt INTM

ERTM; // Enable Global realtime interrupt DBGM

// Background Loop
for (;;);

Timer0中断处理程序为:

#pragma CODE_SECTION(TimerIsr0,"ramfuncs");
__interrupt void TimerIsr0(void) // 2kHz
{
 Counter_500us++;
 if (Counter_500us > 9)
  Counter_5ms++;

PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}

  • 考虑一下PIE有没有正确初始化?

  •  谢谢您的回复。应该不是PIE的配置问题,因为我把CLA相关的程序注释掉后,Timer0的中断就很正常。请问还可能是什么原因呢?

    下面是系统初始化的部分程序:

    void DeviceInit(void)
    {
    WDogDisable(); // Disable the watchdog initially
    DINT; // Global Disable all Interrupts
    IER = 0x0000; // Disable CPU interrupts
    IFR = 0x0000; // Clear all CPU interrupt flags


    // Switch to Internal Oscillator 1 and turn off all other clock
    // sources to minimize power consumption
    EALLOW;
    SysCtrlRegs.CLKCTL.bit.INTOSC1OFF = 0;
    SysCtrlRegs.CLKCTL.bit.OSCCLKSRCSEL=0; // Clk Src = INTOSC1
    SysCtrlRegs.CLKCTL.bit.XCLKINOFF=1; // Turn off XCLKIN
    SysCtrlRegs.CLKCTL.bit.XTALOSCOFF=1; // Turn off XTALOSC
    SysCtrlRegs.CLKCTL.bit.INTOSC2OFF=1; // Turn off INTOSC2
    EDIS;


    // SYSTEM CLOCK speed based on internal oscillator = 10 MHz
    // 0xC = 60 MHz (12)
    // 0xB = 55 MHz (11)
    // 0xA = 50 MHz (10)
    // 0x9 = 45 MHz (9)
    // 0x8 = 40 MHz (8)
    // 0x7 = 35 MHz (7)
    // 0x6 = 30 MHz (6)
    // 0x5 = 25 MHz (5)
    // 0x4 = 20 MHz (4)
    // 0x3 = 15 MHz (3)
    // 0x2 = 10 MHz (2)

    PLLset(0xC); // choose from options above

    // Initialise interrupt controller and Vector Table
    // to defaults for now. Application ISR mapping done later.
    PieCntlInit();
    PieVectTableInit();

    EALLOW; // below registers are "protected", allow access.

    // LOW SPEED CLOCKS prescale register settings
    SysCtrlRegs.LOSPCP.all = 0x0002; // Sysclk / 4 (15 MHz)
    SysCtrlRegs.XCLK.bit.XCLKOUTDIV=2;


    // ADC CALIBRATION
    //---------------------------------------------------
    // The Device_cal function, which copies the ADC & oscillator calibration values
    // from TI reserved OTP into the appropriate trim registers, occurs automatically
    // in the Boot ROM. If the boot ROM code is bypassed during the debug process, the
    // following function MUST be called for the ADC and oscillators to function according
    // to specification.

    SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1; // Enable ADC peripheral clock
    (*Device_cal)(); // Auto-calibrate from TI OTP
    SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 0; // Return ADC clock to original state


    // PERIPHERAL CLOCK ENABLES
    //---------------------------------------------------
    // If you are not using a peripheral you may want to switch
    // the clock off to save power, i.e. set to =0
    //
    // Note: not all peripherals are available on all 280x derivates.
    // Refer to the datasheet for your particular device.

    SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1; // ADC
    //------------------------------------------------
    SysCtrlRegs.PCLKCR3.bit.COMP1ENCLK = 1; // COMP1
    SysCtrlRegs.PCLKCR3.bit.COMP2ENCLK = 1; // COMP2
    SysCtrlRegs.PCLKCR3.bit.COMP3ENCLK = 1; // COMP3
    //------------------------------------------------
    SysCtrlRegs.PCLKCR1.bit.ECAP1ENCLK = 0; //eCAP1
    //------------------------------------------------
    SysCtrlRegs.PCLKCR0.bit.ECANAENCLK=0; // eCAN-A
    //------------------------------------------------
    SysCtrlRegs.PCLKCR1.bit.EQEP1ENCLK = 0; // eQEP1
    //------------------------------------------------
    SysCtrlRegs.PCLKCR1.bit.EPWM1ENCLK = 1; // ePWM1
    SysCtrlRegs.PCLKCR1.bit.EPWM2ENCLK = 1; // ePWM2
    SysCtrlRegs.PCLKCR1.bit.EPWM3ENCLK = 1; // ePWM3
    SysCtrlRegs.PCLKCR1.bit.EPWM4ENCLK = 1; // ePWM4
    SysCtrlRegs.PCLKCR1.bit.EPWM5ENCLK = 1; // ePWM5
    SysCtrlRegs.PCLKCR1.bit.EPWM6ENCLK = 1; // ePWM6
    SysCtrlRegs.PCLKCR1.bit.EPWM7ENCLK = 0; // ePWM7
    SysCtrlRegs.PCLKCR0.bit.HRPWMENCLK = 0; // HRPWM
    //------------------------------------------------
    SysCtrlRegs.PCLKCR0.bit.I2CAENCLK = 1; // I2C
    //------------------------------------------------
    SysCtrlRegs.PCLKCR0.bit.LINAENCLK = 0; // LIN-A
    //------------------------------------------------
    SysCtrlRegs.PCLKCR3.bit.CLA1ENCLK = 1; // CLA1
    //------------------------------------------------
    SysCtrlRegs.PCLKCR0.bit.SCIAENCLK = 1; // SCI-A
    //------------------------------------------------
    SysCtrlRegs.PCLKCR0.bit.SPIAENCLK = 0; // SPI-A
    SysCtrlRegs.PCLKCR0.bit.SPIBENCLK = 0; // SPI-B
    //------------------------------------------------
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Enable TBCLK
    //------------------------------------------------


    //--------------------------------------------------------------------------------------
    // GPIO (GENERAL PURPOSE I/O) CONFIG
    //--------------------------------------------------------------------------------------
    //-----------------------
    // QUICK NOTES on USAGE:
    //-----------------------
    // If GpioCtrlRegs.GP?MUX?bit.GPIO?= 1, 2 or 3 (i.e. Non GPIO func), then leave
    // rest of lines commented
    // If GpioCtrlRegs.GP?MUX?bit.GPIO?= 0 (i.e. GPIO func), then:
    // 1) uncomment GpioCtrlRegs.GP?DIR.bit.GPIO? = ? and choose pin to be IN or OUT
    // 2) If IN, can leave next to lines commented
    // 3) If OUT, uncomment line with ..GPACLEAR.. to force pin LOW or
    // uncomment line with ..GPASET.. to force pin HIGH or
    //--------------------------------------------------------------------------------------
    //--------------------------------------------------------------------------------------
    // GPIO-00 - PIN FUNCTION = SEPIC-PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // 0=GPIO, 1=EPWM1A, 2=Resv, 3=Resv
    // GpioCtrlRegs.GPADIR.bit.GPIO0 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO0 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO0 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-01 - PIN FUNCTION = PWM 1B
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 0; // 0=GPIO, 1=EPWM1B, 2=Resv, 3=COMP1OUT
    GpioCtrlRegs.GPADIR.bit.GPIO1 = 1; // 1=OUTput, 0=INput
    GpioDataRegs.GPACLEAR.bit.GPIO1 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO1 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-02 - PIN FUNCTION = LED String 1 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0; // 0=GPIO, 1=EPWM2A, 2=Resv, 3=Resv
    GpioCtrlRegs.GPADIR.bit.GPIO2 = 1; // 1=OUTput, 0=INput
    GpioDataRegs.GPACLEAR.bit.GPIO2 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO2 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-03 - PIN FUNCTION = LED String 2 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // 0=GPIO, 1=EPWM2B, 2=SPISOMI-A, 3=COMP2OUT
    // GpioCtrlRegs.GPADIR.bit.GPIO3 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO3 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO3 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-04 - PIN FUNCTION = LED String 3 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // 0=GPIO, 1=EPWM3A, 2=Resv, 3=Resv
    // GpioCtrlRegs.GPADIR.bit.GPIO4 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO4 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO4 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-05 - PIN FUNCTION = LED String 4 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // 0=GPIO, 1=EPWM3B, 2=SPISIMO-A, 3=ECAP1
    // GpioCtrlRegs.GPADIR.bit.GPIO5 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO5 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO5 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-06 - PIN FUNCTION = LED String 5 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1; // 0=GPIO, 1=EPWM4A, 2=SYNCI, 3=SYNCO
    // GpioCtrlRegs.GPADIR.bit.GPIO6 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO6 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO6 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-07 - PIN FUNCTION = LED String 6 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1; // 0=GPIO, 1=EPWM4B, 2=SCIRX-A, 3=Resv
    // GpioCtrlRegs.GPADIR.bit.GPIO7 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO7 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO7 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-08 - PIN FUNCTION = LED String 7 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1; // 0=GPIO, 1=EPWM5A, 2=Resv, 3=ADCSOC-A
    // GpioCtrlRegs.GPADIR.bit.GPIO8 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO8 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO8 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-09 - PIN FUNCTION = LED String 8 PWM
    GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1; // 0=GPIO, 1=EPWM5B, 2=LINTX-A, 3=Resv
    // GpioCtrlRegs.GPADIR.bit.GPIO9 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO9 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO9 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-10 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 0; // 0=GPIO, 1=EPWM6A, 2=Resv, 3=ADCSOC-B
    GpioCtrlRegs.GPADIR.bit.GPIO10 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO10 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO10 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-11 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 0; // 0=GPIO, 1=EPWM6B, 2=LINRX-A, 3=Resv
    GpioCtrlRegs.GPADIR.bit.GPIO11 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO11 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO11 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-12 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 0; // 0=GPIO, 1=TZ1, 2=SCITX-A, 3=SPISIMO-B
    GpioCtrlRegs.GPADIR.bit.GPIO12 = 1; // 1=OUTput, 0=INput
    GpioDataRegs.GPACLEAR.bit.GPIO12 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO12 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-13 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 0; // 0=GPIO, 1=TZ2, 2=Resv, 3=SPISOMI-B
    GpioCtrlRegs.GPADIR.bit.GPIO13 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO13 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO13 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-14 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 0; // 0=GPIO, 1=TZ3, 2=LINTX-A, 3=SPICLK-B
    GpioCtrlRegs.GPADIR.bit.GPIO14 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO14 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO14 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-15 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 0; // 0=GPIO, 1=TZ1, 2=LINRX-A, 3=SPISTE-B
    GpioCtrlRegs.GPADIR.bit.GPIO15 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO15 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO15 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    //--------------------------------------------------------------------------------------
    // GPIO-16 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 0; // 0=GPIO, 1=SPISIMO-A, 2=Resv, 3=TZ2
    GpioCtrlRegs.GPADIR.bit.GPIO16 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO16 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO16 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-17 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 0; // 0=GPIO, 1=SPISOMI-A, 2=Resv, 3=TZ3
    GpioCtrlRegs.GPADIR.bit.GPIO17 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO17 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO17 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-18 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 0; // 0=GPIO, 1=SPICLK-A, 2=LINTX-A, 3=XCLKOUT
    GpioCtrlRegs.GPADIR.bit.GPIO18 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO18 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO18 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-19 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 0; // 0=GPIO, 1=SPISTE-A, 2=LINRX-A, 3=ECAP1
    GpioCtrlRegs.GPADIR.bit.GPIO19 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO19 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO19 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-20 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO20 = 0; // 0=GPIO, 1=EQEPA-1, 2=Resv, 3=COMP1OUT
    GpioCtrlRegs.GPADIR.bit.GPIO20 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO20 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO20 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-21 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO21 = 0; // 0=GPIO, 1=EQEPB-1, 2=Resv, 3=COMP2OUT
    GpioCtrlRegs.GPADIR.bit.GPIO21 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO21 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO21 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-22 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 0; // 0=GPIO, 1=EQEPS-1, 2=Resv, 3=LINTX-A
    GpioCtrlRegs.GPADIR.bit.GPIO22 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO22 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO22 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-23 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 0; // 0=GPIO, 1=EQEPI-1, 2=Resv, 3=LINRX-A
    GpioCtrlRegs.GPADIR.bit.GPIO23 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO23 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO23 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-24 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 0; // 0=GPIO, 1=ECAP1, 2=Resv, 3=SPISIMO-B
    GpioCtrlRegs.GPADIR.bit.GPIO24 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO24 = 1; // uncomment if --> Set Low initially
    GpioDataRegs.GPASET.bit.GPIO24 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-25 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=SPISOMI-B
    GpioCtrlRegs.GPADIR.bit.GPIO25 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO25 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO25 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-26 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=SPICLK-B
    GpioCtrlRegs.GPADIR.bit.GPIO26 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO26 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO26 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-27 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=SPISTE-B
    GpioCtrlRegs.GPADIR.bit.GPIO27 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO27 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO27 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-28 - PIN FUNCTION = SCI-RX
    GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // 0=GPIO, 1=SCIRX-A, 2=I2CSDA-A, 3=TZ2
    // GpioCtrlRegs.GPADIR.bit.GPIO28 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO28 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO28 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-29 - PIN FUNCTION = SCI-TX
    GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // 0=GPIO, 1=SCITXD-A, 2=I2CSCL-A, 3=TZ3
    // GpioCtrlRegs.GPADIR.bit.GPIO29 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO29 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO29 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-30 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 0; // 0=GPIO, 1=CANRX-A, 2=Resv, 3=Resv
    GpioCtrlRegs.GPADIR.bit.GPIO30 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO30 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPASET.bit.GPIO30 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-31 - PIN FUNCTION = LED2 on controlCARD
    GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 0; // 0=GPIO, 1=CANTX-A, 2=Resv, 3=Resv
    GpioCtrlRegs.GPADIR.bit.GPIO31 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPACLEAR.bit.GPIO31 = 1; // uncomment if --> Set Low initially
    GpioDataRegs.GPASET.bit.GPIO31 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    //--------------------------------------------------------------------------------------
    // GPIO-32 - PIN FUNCTION = I2CSDA
    GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1; // 0=GPIO, 1=I2CSDA-A, 2=SYNCI, 3=ADCSOCA
    // GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO32 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPBSET.bit.GPIO32 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-33 - PIN FUNCTION = PFC-DrvEnable
    GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 1; // 0=GPIO, 1=I2CSCL-A, 2=SYNCO, 3=ADCSOCB
    // GpioCtrlRegs.GPBDIR.bit.GPIO33 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO33 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPBSET.bit.GPIO33 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-34 - PIN FUNCTION = LED3 on controlCARD
    GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=Resv
    GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO34 = 1; // uncomment if --> Set Low initially
    GpioDataRegs.GPBSET.bit.GPIO34 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    //--------------------------------------------------------------------------------------
    // GPIO 35-38 are defaulted to JTAG usage, and are not shown here to enforce JTAG debug
    // usage.
    //--------------------------------------------------------------------------------------
    //--------------------------------------------------------------------------------------
    // GPIO-39 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPBMUX1.bit.GPIO39 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=Resv
    GpioCtrlRegs.GPBDIR.bit.GPIO39 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO39 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPBSET.bit.GPIO39 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-40 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPBMUX1.bit.GPIO40 = 0; // 0=GPIO, 1=EPWM7A, 2=Resv, 3=Resv
    GpioCtrlRegs.GPBDIR.bit.GPIO40 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO40 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPBSET.bit.GPIO40 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-41 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 0; // 0=GPIO, 1=EPWM7B, 2=Resv, 3=Resv
    GpioCtrlRegs.GPBDIR.bit.GPIO41 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO41 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPBSET.bit.GPIO41 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-42 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPBMUX1.bit.GPIO42 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=COMP1OUT
    GpioCtrlRegs.GPBDIR.bit.GPIO42 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO42 = 1; // uncomment if --> Set Low initially
    GpioDataRegs.GPBSET.bit.GPIO42 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-43 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPBMUX1.bit.GPIO43 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=COMP2OUT
    GpioCtrlRegs.GPBDIR.bit.GPIO43 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO43 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPBSET.bit.GPIO43 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    // GPIO-44 - PIN FUNCTION = --Spare--
    GpioCtrlRegs.GPBMUX1.bit.GPIO44 = 0; // 0=GPIO, 1=Resv, 2=Resv, 3=Resv
    GpioCtrlRegs.GPBDIR.bit.GPIO44 = 0; // 1=OUTput, 0=INput
    // GpioDataRegs.GPBCLEAR.bit.GPIO44 = 1; // uncomment if --> Set Low initially
    // GpioDataRegs.GPBSET.bit.GPIO44 = 1; // uncomment if --> Set High initially
    //--------------------------------------------------------------------------------------
    //--------------------------------------------------------------------------------------
    EDIS; // Disable register access
    }

    void PieCntlInit(void)
    {
    // Disable Interrupts at the CPU level:
    DINT;

    // Disable the PIE
    PieCtrlRegs.PIECTRL.bit.ENPIE = 0;

    // Clear all PIEIER registers:
    PieCtrlRegs.PIEIER1.all = 0;
    PieCtrlRegs.PIEIER2.all = 0;
    PieCtrlRegs.PIEIER3.all = 0;
    PieCtrlRegs.PIEIER4.all = 0;
    PieCtrlRegs.PIEIER5.all = 0;
    PieCtrlRegs.PIEIER6.all = 0;
    PieCtrlRegs.PIEIER7.all = 0;
    PieCtrlRegs.PIEIER8.all = 0;
    PieCtrlRegs.PIEIER9.all = 0;
    PieCtrlRegs.PIEIER10.all = 0;
    PieCtrlRegs.PIEIER11.all = 0;
    PieCtrlRegs.PIEIER12.all = 0;

    // Clear all PIEIFR registers:
    PieCtrlRegs.PIEIFR1.all = 0;
    PieCtrlRegs.PIEIFR2.all = 0;
    PieCtrlRegs.PIEIFR3.all = 0;
    PieCtrlRegs.PIEIFR4.all = 0;
    PieCtrlRegs.PIEIFR5.all = 0;
    PieCtrlRegs.PIEIFR6.all = 0;
    PieCtrlRegs.PIEIFR7.all = 0;
    PieCtrlRegs.PIEIFR8.all = 0;
    PieCtrlRegs.PIEIFR9.all = 0;
    PieCtrlRegs.PIEIFR10.all = 0;
    PieCtrlRegs.PIEIFR11.all = 0;
    PieCtrlRegs.PIEIFR12.all = 0;
    }


    void PieVectTableInit(void)
    {
    int16 i;
    Uint32 *Source = (void *) &ISR_ILLEGAL;
    Uint32 *Dest = (void *) &PieVectTable;

    EALLOW;
    for(i=0; i < 128; i++)
    *Dest++ = *Source;
    EDIS;

    // Enable the PIE Vector Table
    PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
    }

  • 大神帮忙看看可能是什么原因啊?

  • http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/555405?tisearch=e2e-sitesearch&keymatch=interrupt%200x3ff599

    参考一下这个帖子,看看有没有可能是存储空间分配以及使用权的问题