This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335外接AD7657问题

Other Parts Discussed in Thread: ADS8557

大家好,有个问题请帮忙看下

之前有项目C28345+AD7657,参照官方的C28343 control card的并行接法,

现在打算用F28335+AD7657,F28335的SPI串行口已经被其它外设资源占用,

这种情形下要使用AD的并行接法的话,是不是只能用F28335的GPIO来连AD7657控制信号和并行数据信号,或者是否有其它方式?

如果用GPIO控制的并行方式,从GPIO获得一个16位完整的并行数据时间要多久,如何计算?(我怕这种方式获取数据的时间太久,满足不了系统要求)。

另外,是否可以把AD假设为外部扩展的存储芯片来设计,使用F28335的外部存储接口来并行连接AD7657?