This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812输出时钟



我现在给2812外扩AD,需要提供10MHZ的时钟信号,想使用DSP的时钟信号,查到XCLKOUT引脚可以输出时钟信号。但是用示波器测了一下,这个引脚输出的是40几MHZ的三角波信号,幅值有1V左右,叠加了一个直流电平。我想问一下,DSP的这个引脚可以输出10MHZ的时钟信号吗?怎样才能输出矩形脉冲信号?

  • 龙辉,

    XCLKOUT只能设置成SYSCLKOUT, SYSCLKOUT/2, SYSCLKOUT/4

    至于为什么是三角波,我想主要原因是示波器通道的问题。

    另外,这种与芯片相关的一些资料,查数据手册自己都能解决。得对你要求高一点!

  • 谢谢蝈蝈了。

    我查过手册,正如你所说的,最小只能设定为系统时钟的1/4,我就想着会不会有其他我不知道的方案,所以想请教一下。

    原来想着系统30MHZ晶振,经过倍频以后才到150MHZ,如果我采样的时候不倍频,系统时钟就是30MHZ,那么经过分频就可以达到比较低的频率了,等采集完成后,再将系统的主频倍频上去。但是担心这样做的后果是导致系统不稳定以及其他问题。

    我知道,你这是为我好,想让我自己学会解决问题的方法。谢谢你啊,蝈蝈!