This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
28335的QEP模块计算转速,可是手动转动电机时QPOSCNT寄存器的计数值只有0,1,2,3,9999,10000这几个数值,而且也不是顺序跳变的。寄存器的配置没什么问题,输入的ABZ信号,电平低电平是0.8V,高电平3.5V左右,不知道是不是这个电平范围的问题影响捕获计数。
还有我想问下28335的QEP模块输入电平范围是多少,5V的ABZ可以直接输入吗?
我整形后0.4-3.6V,这个电平可以吗?
我现在是手转电机计数正常,但是上电运行后计数就不正常。