This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

drv8301 revd 运算放大电路1.65V偏移问题

Other Parts Discussed in Thread: TLV2781上电时候测试电流反馈1.65V偏置是什么意思啊?是指DSP上电瞬间就会自动增加1.65V,以把测得的电流信号–1.65V~+1.65V偏置为0~3.3V提供给DSP处理。但是我现在自己仿照drv8301revd做了电路板,经过测试,当电机启动前:如果TLV2781输出端电压在1.65V附近(1.645~1.655V)时电机可以正常启动,可以输出额定扭矩。但是有的电路板的TLV2781输出电压远离1.65V,比如说:1.62V,此时电机可能无法正常启动,就算启动后也不能输出额定扭矩,明显感觉电机出力降低,替换TLV2781后输出端电压可能在1.65V附近,此时电机启动和带载能力都正常。 1、请问怎么处理在TLV2781输出端远离1.65V时无法启动和带载能力下降问题?非常感谢!
  • 好像与半桥驱动的开启有关    其中的一个VREF

    这个降低了   可能H桥开启不好了   效率低了

  • 我的意思是怎么解决运放TLV2781偏离1.65V时的解决合理方案,希望高人指导下?⑴替换运放后只要输出在1.65V附近即可解决该问题,但是替换运放硬件成本太高,且浪费时间,这个方案肯定不行。⑵TLV2781在输入1.65V时,输出在1.62V~1.675V(实际应该输出1.65V)范围内,是不是这个运放精度太低了,相差55mv。
  • 1.62V~1.675的偏差不是因为运放精度导致的,可能是电源,可能是分压电路。

    所以在马达启动之前,还是需要计算Offset的,在FOC计算的时候把offset减掉即可,即便是1.62V~1.675V有偏差,也没有问题。

  • 正常來說

    你應該在訊號輸出前(開機狀態下),先讀取ADC確認Offset值

    再將offset與你的ADC轉成電壓相關的運算式做調整

  • 这个偏差确实是运放导致,替换运放TLV2781(这里的替换是指替换后的运放还是运放TLV2781)输出1.65V正常,如果不替换电机启动就会一直处于异常状态。我已经按照实际测试的1.62V作为offset减去,还是不能改善启动抖动(采样时电压为1.62V+电机电流*采样电阻,最后再把采样得到的值减去1.62V,这样处理还是无法消除启动抖动),这是什么原因?
  • 我替换分压电路的电阻,无法使输出达到1.65V ,这样是不是还是不能排除运放TLV2781有问题?