This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

依照TI的高压套件HVKIT,采用28069芯片,自己重新设计了新板子,使用外部参考电压3.0v,motorware例程里面的软件应该怎样更改设置?

Other Parts Discussed in Thread: MOTORWARE

如题,采用instaspinFoc方案,硬件上 自己重新设计了电路板,与demo板不同的是,自己设计的新板adc参考电压上采用了外部3.0v(demo板是内部3.3v),软件还是采用motorware里面的例程,在例程里我只找到了选择外部或者内部参考电压的设置,但是没有找到更改电压数值的设置, 例如在软件里是否有个地方需要将ADC参考电压的数值由3.3v改为3.0v 。 新手菜鸟,求各位大神指点。

  • 如题,采用instaspinFoc方案,硬件上 自己重新设计了电路板,与demo板不同的是,自己设计的新板adc参考电压上采用了外部3.0v(demo板是内部3.3v),软件还是采用motorware里面的例程,在例程里我只找到了选择外部或者内部参考电压的设置,但是没有找到更改电压数值的设置, 例如在软件里是否有个地方需要将ADC参考电压的数值由3.3v改为3.0v 。 新手菜鸟,求各位大神指点。

    ERIC:

    你只要配置为外部参考电压就可以啦。这样当3V模拟信号输入时,即为满量程4095. 

    注意user.h里面的电压电流满量程对应的值也都要用3V来算。