本人用仿真器XDS100V3为隔离型,在CCS6.2的环境下仿真下载28377D的程序进行在线仿真工作,该下载过程比较慢,不知道是怎么回事?如何提高下载速度?请高手指点。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本人用仿真器XDS100V3为隔离型,在CCS6.2的环境下仿真下载28377D的程序进行在线仿真工作,该下载过程比较慢,不知道是怎么回事?如何提高下载速度?请高手指点。。。
Seven,你好!谢谢你的指导,针对“The Debug Probe 1149.1 Frequency”一栏选择“Adaptive with user specified limit”,然后在“Enter a value from 488Hz to 30.0MHz”一栏填入30.0MHz。系统此处默认时是1MHz。更改后就针对测试的代码烧录而言从140s时间缩短为110s时间。
另:上面Eric提到更换为XDS510的话也可以提升下载速度,只是有一个疑问:CCS6.2的仿真器驱动不是默认安装了的么?如果是的话,目前.ccxml文件中的仿真器选项还没有XDS510的。主要还是XDS100,XDS2XX以及XDS560,请明确下,谢谢!
您好!
不同XDS系列仿真器的性能对比可以参考以下网页:
http://processors.wiki.ti.com/index.php/XDS_Performance_comparison
你这个资料信息太及时了,提供的测试数据的对比很有说明力,谢谢。