This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377S的CLA



官方例程cla_adc_fir32怎么进不了中断,

__interrupt void cla1Isr7 ()
{
    //
    // Clear the ADC interrupt flag so the next SOC can occur
    // Clear the PIEACK bits so another interrupt can be taken
    //
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
    PieCtrlRegs.PIEACK.all = (PIEACK_GROUP1 | PIEACK_GROUP11);

    //
    // Read the raw ADC RESULT1 register value and
    // put it into the AdcBuf buffer
    // This can be compared to the CLA filtered value
    //
    AdcBuf[SampleCount] = AdcaResultRegs.ADCRESULT0;

    //
    // Read the CLA filtered value and put it in the
    // AdcFiltBuf buffer
    //
    AdcFiltBuf[SampleCount] = voltFilt;

    //
    // Make sure that the buffer does not overflow
    // the buffer size.  If it is larger than ADC_BUF_LEN
    // then rewind back to the sample 0
    //
    SampleCount++;
    if( SampleCount == ADC_BUF_LEN )
    {
        SampleCount = 0;
    }

    //
    // Uncomment to halt debugger here
    //
//    asm(" ESTOP0");
}

我在这里打断点一直进不去,为什么呢?