This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2833ADC 双排序器Start/Stop模式

Other Parts Discussed in Thread: CONTROLSUITE

有个问题!

关于28335ADC的 Sequencer Start/Stop模式,在TI28335 ADC 参考手册第22页,如下图:

代码初始化:

1. eWPM1计数器工作在up-down模式;

2. CTR=0时,产生ePWM1SOCA触发AD排序器1采样转换I1,I2,I3这三个通道;

3. CTR=PRD时,产生ePWM1SOCB触发AD排序器2采样转换V1,V2,V3这三个通道;

但为什么转换的结果只有I1,I2,I3这三个通道转换成功了,而V1,V2,V3折三个通道始终值为0。

请问大家使用过这种模式吗?

麻烦大家给指导指导吧!!

测试代码如下:

附件中是源文件!

#include "DSP2833x_Device.h"     // DSP2833x Headerfile Include File

#include "DSP2833x_Examples.h"   // DSP2833x Examples Include File

// Prototype statements for functions found within this file.

interrupt void  adc_isr(void);

Uint16 VoltageA[3];

Uint16 VoltageB[3];

Uint16 upDownFlag = 0;

Uint16 PWMDuty = 0;

void main(void)

{

InitSysCtrl();

DINT;

InitPieCtrl();

IER = 0x0000;

IFR = 0x0000;

InitPieVectTable();

InitEPwm1Gpio(); //PWM outPin≥ı ºªØ

EALLOW;

GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 0; // GPIO0∏¥”√Œ™GPIO𶃋

GpioCtrlRegs.GPADIR.bit.GPIO7 = 1;  // GPIO0…Ë÷√Œ™ ‰≥ˆ

PieVectTable.ADCINT = &adc_isr; //ADC interrupt

PieVectTable.EPWM1_INT = &EPWM1_INT_ISR; //ePWM1 zero interrupt

EDIS;

AdcRegs.ADCTRL1.all = 0;

    AdcRegs.ADCTRL2.all = 0;

    AdcRegs.ADCTRL3.all = 0;

    //config ADC

    AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;

    AdcRegs.ADCTRL2.bit.RST_SEQ2 = 1;

    AdcRegs.ADCTRL1.bit.ACQ_PS = 3;

    AdcRegs.ADCTRL1.bit.SEQ_CASC = 0; //0:À´≈≈–Ú∆˜ƒ£ Ω£ª1£∫º∂¡™≈≈–Úƒ£ Ω

    AdcRegs.ADCTRL3.bit.SMODE_SEL = 0; //0:¡¨–¯≤…—˘£ª1£∫Õ¨≤Ω≤…—˘ƒ£ Ω

    AdcRegs.ADCTRL1.bit.CONT_RUN = 0; //0£∫∆Ù∂Ø/Õ£÷πƒ£ Ω£ª1:¡¨–¯ƒ£ Ω

    AdcRegs.ADCTRL1.bit.SEQ_OVRD = 0;

    //config SEQ1

    AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 1;

    AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;

    AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1;

    AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x00;

    AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x01;

    AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x02;

    AdcRegs.ADCMAXCONV.all = 0x22;

    //config SEQ2

    AdcRegs.ADCTRL2.bit.SOC_SEQ2 = 1;

    AdcRegs.ADCTRL2.bit.EPWM_SOCB_SEQ2 = 1;

    AdcRegs.ADCTRL2.bit.INT_ENA_SEQ2 = 1;

    AdcRegs.ADCCHSELSEQ3.bit.CONV08 = 0x08;

AdcRegs.ADCCHSELSEQ3.bit.CONV09 = 0x09;

AdcRegs.ADCCHSELSEQ3.bit.CONV10 = 0x0A;

// AdcRegs.ADCMAXCONV.bit.MAX_CONV2 = 0x2;

extern void DSP28x_usDelay(Uint32 Count);

AdcRegs.ADCTRL3.all |= 0x00E0;  // Power up bandgap/reference/ADC circuits

DELAY_US(5000L);         // Delay before converting ADC channels

/*ePWM config*/

EPwm1Regs.TBPRD = 6000;               // ±ª˘º∆ ˝÷‹∆

EPwm1Regs.CMPA.half.CMPA = 1500;         //º∆ ˝±»Ωœºƒ¥Ê∆˜A

EPwm1Regs.TBPHS.all = 0; // ±ª˘Õ¨≤Ωœ‡Œª

EPwm1Regs.TBCTR = 0; // ±ª˘º∆ ˝∆˜≥ı º÷µ

EPwm1Regs.TBCTL.bit.PHSDIR = TB_UP; //œ‡Œª∑ΩœÚøÿ÷∆ºƒ¥Ê∆˜£¨µ±Õ¨≤Ω–≈∫≈¿¥ ±£¨◊∞‘ÿ¡Àœ‡Œªºƒ¥Ê∆˜µƒ÷µ∫Û «œÚ…œº∆ ˝ªπ «œÚœ¬º∆ ˝

EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; //œ‡ŒªÕ¨≤Ω–≈∫≈‘¥—°‘Ò£¨µ±CTR=ZERO ± ‰≥ˆÕ¨≤Ω–≈∫≈

EPwm1Regs.TBCTL.bit.PHSEN = TB_ENABLE; //µ±Õ¨≤Ω–≈∫≈¿¥ ±£¨øÿ÷∆ «∑Ò◊∞‘ÿœ‡Œªºƒ¥Ê∆˜µƒ÷µ--µ±Õ¨≤Ω–≈∫≈¿¥ ±£¨º∆ ˝ºƒ¥Ê∆˜◊∞‘ÿœ‡Œªºƒ¥Ê∆˜µƒ÷µ

EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; //Ω˚÷π π”√”∞◊”ºƒ¥Ê∆˜

EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; //º∆ ˝ƒ£ Ωøÿ÷∆ºƒ¥Ê∆˜:up; down; up-down;stop

EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; //∏flÀŸ ±ª˘ ±÷”∑÷∆µ

EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1; // ±ª˘ ±÷”∑÷∆µ

EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL; //À¿«¯ƒ£øÈ ‰»Î‘¥øÿ÷∆£¨Ω´ePWM3A◊˜Œ™À´±fl—ÿ—” ± ‰»Î‘¥

EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //À¿«¯º´–‘—°‘Òøÿ÷∆£¨ePWM3A≤ª∑≠◊™£¨ePWM3B∑≠◊™

EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;

EPwm1Regs.DBRED = 100; //À¿«¯…œ…˝—ÿ—” ±ºƒ¥Ê∆˜

EPwm1Regs.DBFED = 100; //À¿«¯œ¬Ωµ—ÿ—” ±ºƒ¥Ê∆˜

EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR;        //µ± ±ª˘º∆ ˝∆˜µƒ÷µµ»”0 ±£¨ePWM3A ‰≥ˆµÕ

EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; //µ± ±ª˘º∆ ˝∆˜œÚ…œº∆ ˝£¨≤¢«“ ±ª˘º∆ ˝∆˜µƒ÷µ”ÎCMPAºƒ¥Ê∆˜µƒ÷µœ‡µ» ±£¨ePWMA ‰≥ˆ∏fl

EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR; //µ± ±ª˘º∆ ˝∆˜œÚœ¬º∆ ˝£¨≤¢«“ ±ª˘º∆ ˝∆˜µƒ÷µ”ÎCMPAºƒ¥Ê∆˜µƒ÷µœ‡µ» ±£¨eWPMA ‰≥ˆµÕ

EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_PRD; //ePWMxSOCA¥•∑¢–≈∫≈≤˙…˙Ãıº˛£¨µ±CTR=0 ±≤˙…˙÷–∂œ¥•∑¢

EPwm1Regs.ETSEL.bit.SOCAEN = 0x1; // πƒ‹ePWMxSOCA–≈∫≈≤˙…˙

EPwm1Regs.ETSEL.bit.SOCBEN = 0x1; // πƒ‹ePWMxSOCB–≈∫≈≤˙…˙

EPwm1Regs.ETSEL.bit.SOCBSEL = ET_CTR_ZERO; //ePWMxSOCB¥•∑¢–≈∫≈≤˙…˙Ãıº˛£¨µ±CTR=PRD ±≤˙…˙÷–∂œ¥•∑¢

EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; //ePWM÷–∂œÃıº˛—°‘Ò

EPwm1Regs.ETSEL.bit.INTEN = 0x1; // πƒ‹ePWM÷–∂œ

EPwm1Regs.ETPS.bit.SOCACNT = 0x1; //∂‘≤˙…˙ePWMxSOCAÃıº˛ ¬º˛º∆ ˝£¨”–1¥Œ ¬º˛∑¢…˙ ±

EPwm1Regs.ETPS.bit.SOCAPRD = 0x1; //ePWMxSOCA–≈∫≈≤˙…˙Ãıº˛£¨‘µ1∏ˆ ¬º˛ ±£¨≤˙…˙SOC–≈∫≈

EPwm1Regs.ETPS.bit.SOCBCNT = 0x1; //∂‘≤˙…˙ePWMxSOCBÃıº˛ ¬º˛º∆ ˝£¨”–1¥Œ ¬º˛∑¢…˙ ±

EPwm1Regs.ETPS.bit.SOCBPRD = 0x1; //ePWMxSOCB–≈∫≈≤˙…˙Ãıº˛£¨‘µ1∏ˆ ¬º˛ ±£¨≤˙…˙SOC–≈∫≈

EPwm1Regs.ETPS.bit.INTCNT = 0x1; //∂‘ePWM÷–∂œ ¬º˛º∆ ˝

EPwm1Regs.ETPS.bit.INTPRD = 0x1; //÷–∂œ≤˙…˙Ãıº˛…Ë÷√£¨µ±INTCNT º∆ ˝µ»”1 ±£¨≤˙…˙÷–∂œ

EPwm1Regs.ETCLR.bit.INT = 0x1; //«Â≥˝÷–∂œ±Í÷挪

EPwm1Regs.ETCLR.bit.SOCA = 0x1; //«Â≥˝SOCA±Í÷挪

EPwm1Regs.ETCLR.bit.SOCB = 0x1;

//enable Interrupt

    PieCtrlRegs.PIECTRL.bit.ENPIE = 1; //vector enable

    PieCtrlRegs.PIEIER1.bit.INTx6 = 1; //enable adc

    PieCtrlRegs.PIEIER3.bit.INTx1 = 1; //enable ePWM1 zero interrupt

    IER |= M_INT1;

    IER |= M_INT3;

EINT;   // ◊‹÷–∂œ INTM  πƒ‹

ERTM;   //  πƒ‹◊‹ µ ±÷–∂œ DBGM

    while(1)

    {

    DELAY_US(1000);

    }

}

interrupt void  adc_isr(void)

{

GpioDataRegs.GPADAT.bit.GPIO7 = 1;

// Insert ISR Code here

VoltageA[0] = AdcRegs.ADCRESULT0 >>4;

VoltageA[1] = AdcRegs.ADCRESULT1 >>4;

VoltageA[2] = AdcRegs.ADCRESULT2 >>4;

VoltageB[0] = AdcRegs.ADCRESULT3 >>4;

VoltageB[1] = AdcRegs.ADCRESULT4 >>4;

VoltageB[2] = AdcRegs.ADCRESULT5 >>4;

AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;         // Reset SEQ1

AdcRegs.ADCTRL2.bit.RST_SEQ2 = 1;         // Reset SEQ1

AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;       // Clear INT SEQ1 bit

AdcRegs.ADCST.bit.INT_SEQ2_CLR = 1;       // Clear INT SEQ1 bit

PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;   // Acknowledge interrupt to PIE

GpioDataRegs.GPADAT.bit.GPIO7 = 0;

}

  • 您好!

    请到以下网址下载controlSUITE:

    www.ti.com/controlsuite

    (选择offline ZIP installer)

    安装后可以在以下目录下找到F28335的例程:

    C:\ti\controlSUITE\device_support\f2833x\v142\DSP2833x_examples_ccsv5

    可以参考其中adc_开头的例程中的设置.

  • Hi Linda

    谢谢你的回复

    controlSUITE里关于ADC的部分我都看过,里面没有和我需求类似的应用,他们提供的模式和我的需求有很大的不同,比如“Example_2833xAdcSoc.c”的ePWM工作在Up-count 模式,每个PWM周期只产生了一个SOCA作为ADC SEQ1的触发信号。

    而我需要用到的是ePWM工作在Up-down-count模式,在一个PWM周期里会产生SOCA和SOCB两个触发信号触发两次AD转换,且ADC排序器工作在Start/Stop模式,如《TMS320x2833x Analog-to-Digital Converter (ADC) Module》Reference Guide中Example 1-4中的描述,但TI没有提供相关的样例代码,而我自己配置的调试了很久了都不能达到预期的效果,这种模式在电机控制应用中应该是很常用的方式吧,能不能帮我提供一个可参考的样例呢

    谢谢