This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377S

28377S的CAN怎样接受任意ID的帧,官方历程只能接受特定帧

  • 您好,我没有具体例子,建议您调试前先查下datasheet,在以下链接:

    http://www.ti.com/lit/ug/spruhx5e/spruhx5e.pdf 21章节ecan;

  •     sRXCANMessage.ui32MsgID = 1;                                           // CAN message ID - use 1
        sRXCANMessage.ui32MsgIDMask = 0;                                  // no mask needed for TX
        sRXCANMessage.ui32Flags = MSG_OBJ_NO_FLAGS;
        sRXCANMessage.ui32MsgLen = sizeof(ucRXMsgData);   // size of message is 4
        sRXCANMessage.pucMsgData = ucRXMsgData;                // ptr to message content

        //
        // Setup the message object being used to receive messages
        //
        CANMessageSet(CANA_BASE, 2, &sRXCANMessage, MSG_OBJ_TYPE_RX);

    只能接收ID等于1的CAN帧,怎样改为接收任意ID的帧

  • 我也遇到相同的问题,请问如何配置能接收所有ID的CAN报文