This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377D中PWM输出问题



如图,1代表T1管,3代表T3管,2代表T2管,4代表T4管,1、3互补,分别由PWM1A和PWM1B驱动,2、4互补,分别由PWM2A和PWM2B驱动;且1和4属于主开关管,2、3属于T型的横管。在28377D的EPWM初始配置中,各管输出均强制拉低;在调试过程中,给固定的CMPA值,发现pwm使能输出时,第一个脉冲会造成1和4直通的情况,之后的脉冲输出是正常的,请问造成这种现象的原因以及如何解决此问题?谢谢!

  • 如图,1代表T1管,3代表T3管,2代表T2管,4代表T4管,1、3互补,分别由PWM1A和PWM1B驱动,2、4互补,分别由PWM2A和PWM2B驱动;且1和4属于主开关管,2、3属于T型的横管。在28377D的EPWM初始配置中,各管输出均强制拉低;在调试过程中,给固定的CMPA值,发现pwm使能输出时,第一个脉冲会造成1和4直通的情况,之后的脉冲输出是正常的,请问造成这种现象的原因以及如何解决此问题?谢谢!

    Eric:

    看你的波形,其实PWM工作并没有异常,T1,T3还是互补,T2,T4也是互补,你并没有规定T1,T4不能直通。

    如果你对第一个脉冲有疑问,那你就得看一下你使能PWM的时候,这两个PWM模块比较寄存器里面的值,周期值,计数值分别是什么。