This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377s关于sci通讯的问题



注意到GPIO72和84用来设置BOOT MODE,不接仿真器时通过检测其电平选择BOOT模式

而SCIA的两个TXD和RXD可以分别为84和85脚,这样使用的话是否会冲突

另外注意到在launchpad的原理图中,别的引脚也可配置为SCITXDA与SCIRXDA,如GPIO42和43,但是我在28377的用户手册中并未找到相关的操作配置方法

目前进行的工作是画一块28377的pcb板,遇到以上问题很疑惑,希望得到解答,万谢1