This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大致情况如下:
使用了xds100V1和xds100v3仿真器连接自己做的一款板子,均能连接上,而且也能烧进flash,但是我的DSP板子无法输出PWM。而当我使用TI的Launchpad烧程序的时候,测试相应引脚是有PWM输出的。
相关器件及测试如下:
1.DSP型号为TMS320F28027,DSP板自己做的;
2.使用5V供电,利用AMS117转成3.3V(输出和输入端均用一个105和106的电容并联),实际电压3.08V左右(测试的是第十一个引脚);
3.仿真器为xds100v1和xds100v3(隔离型);
4.测试了48个引脚,没发现虚焊。
5.曾怀疑是3.3V的原因,在AMS1117的输出端直接接了一个3.3V供电,限流900mA,但是再次烧录,还是无PWM输出。
请问,还有那些原因可能导致DSP无法输出PWM(除了相应的GPIO口损坏的情况下)?