void InitXintf(void)
{
// This shows how to write to the XINTF registers. The
// values used here are the default state after reset.
// Different hardware will require a different configuration.
// For an example of an XINTF configuration used with the
// F28335 eZdsp, refer to the examples/run_from_xintf project.
// Any changes to XINTF timing should only be made by code
// running outside of the XINTF.
// All Zones---------------------------------
// Timing for all zones based on XTIMCLK = 1/2 SYSCLKOUT
EALLOW;
XintfRegs.XINTCNF2.bit.XTIMCLK = 1;
// No write buffering
XintfRegs.XINTCNF2.bit.WRBUFF = 0;
// XCLKOUT is enabled
XintfRegs.XINTCNF2.bit.CLKOFF = 0;
// XCLKOUT = XTIMCLK/2
XintfRegs.XINTCNF2.bit.CLKMODE = 1;
// Zone 0------------------------------------
// When using ready, ACTIVE must be 1 or greater
// Lead must always be 1 or greater
// Zone write timing
/* XintfRegs.XTIMING0.bit.XWRLEAD = 3;
XintfRegs.XTIMING0.bit.XWRACTIVE = 7;
XintfRegs.XTIMING0.bit.XWRTRAIL = 3;
// Zone read timing
XintfRegs.XTIMING0.bit.XRDLEAD = 3;
XintfRegs.XTIMING0.bit.XRDACTIVE = 7;
XintfRegs.XTIMING0.bit.XRDTRAIL = 3;
// double all Zone read/write lead/active/trail timing
XintfRegs.XTIMING0.bit.X2TIMING = 1;
// Zone will sample XREADY signal
XintfRegs.XTIMING0.bit.USEREADY = 1;
XintfRegs.XTIMING0.bit.READYMODE = 1; // sample asynchronous
// Size must be either:
// 0,1 = x32 or
// 1,1 = x16 other values are reserved
XintfRegs.XTIMING0.bit.XSIZE = 3;
*/
// Zone 6------------------------------------
// When using ready, ACTIVE must be 1 or greater
// Lead must always be 1 or greater
// Zone write timing
XintfRegs.XTIMING6.bit.XWRLEAD = 1;
XintfRegs.XTIMING6.bit.XWRACTIVE = 1;
XintfRegs.XTIMING6.bit.XWRTRAIL = 1;
// Zone read timing
XintfRegs.XTIMING6.bit.XRDLEAD = 2;
XintfRegs.XTIMING6.bit.XRDACTIVE = 2;
XintfRegs.XTIMING6.bit.XRDTRAIL = 2;
// double all Zone read/write lead/active/trail timing
XintfRegs.XTIMING6.bit.X2TIMING = 1;
// Zone will sample XREADY signal
XintfRegs.XTIMING6.bit.USEREADY = 1;
XintfRegs.XTIMING6.bit.READYMODE = 0; // sample asynchronous
// Size must be either:
// 0,1 = x32 or
// 1,1 = x16 other values are reserved
XintfRegs.XTIMING6.bit.XSIZE = 3;
// Zone 7------------------------------------
// When using ready, ACTIVE must be 1 or greater
// Lead must always be 1 or greater
// Zone write timing
XintfRegs.XTIMING7.bit.XWRLEAD = 3;
XintfRegs.XTIMING7.bit.XWRACTIVE = 7;
XintfRegs.XTIMING7.bit.XWRTRAIL = 3;
// Zone read timing
XintfRegs.XTIMING7.bit.XRDLEAD = 3;
XintfRegs.XTIMING7.bit.XRDACTIVE = 7;
XintfRegs.XTIMING7.bit.XRDTRAIL = 3;
// double all Zone read/write lead/active/trail timing
XintfRegs.XTIMING7.bit.X2TIMING = 1;
// Zone will sample XREADY signal
XintfRegs.XTIMING7.bit.USEREADY = 1;
XintfRegs.XTIMING7.bit.READYMODE = 1; // sample asynchronous
// Size must be either:
// 0,1 = x32 or
// 1,1 = x16 other values are reserved
XintfRegs.XTIMING7.bit.XSIZE = 3;
// Bank switching
// Assume Zone 7 is slow, so add additional BCYC cycles
// when ever switching from Zone 7 to another Zone.
// This will help avoid bus contention.
XintfRegs.XBANK.bit.BANK = 7;
XintfRegs.XBANK.bit.BCYC = 7;
EDIS;
//Force a pipeline flush to ensure that the write to
//the last register configured occurs before returning.
// InitXintf16Gpio();
// InitXintf32Gpio();
asm(" RPT #7 || NOP");
}