我从28335的书册中看到数AD的电源VDDA2和VSSA2是作为AD输入限幅用了,请问是否就是说AD内部本身有双二极管限幅的电路?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,
你好!
VDDA2和VSSA2分别是ADC模块的电源和地,建议楼主使用时在AD输入管脚外部加入双二极管电路做保护!
C2000的硬件电路设计请参考www.ti.com/.../spraas1b.pdf
楼主,你好!
“ nput clamp current”是指到地和到电源的钳位二极管所能承受的最大电流,请注意注释里持续的值为2mA,因此芯片虽然内带楼主所说的双二极管保护电路,但是由于钳位电流小,因此还是建议在实际应用中,AD的输入管脚外接双二极管保护电路。