谁有ccs2.2的软件包以及安装教程,公司有个老项目需要这个编译器,ccs3.3的编译器编译出来的out文件有问题,想用2.2的编译器编译,我的芯片是tms320f240pqa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谁有ccs2.2的软件包以及安装教程,公司有个老项目需要这个编译器,ccs3.3的编译器编译出来的out文件有问题,想用2.2的编译器编译,我的芯片是tms320f240pqa
load program时出错 显示data verification failed at address 0x44,下面是我的cmd文件:
MEMORY
{
PAGE 0 : VECS : origin = 0000h , length = 40h /* INTERRUPT VECTORS */
PROGM : origin = 0044h , length = 3fbch /* ON CHIP FLASH */
/*//PROGM0 : origin = 22a0h , length = 160h ON CHIP FLASH */
PAGE 1 : B0 : origin = 200h , length = 100h /* ON CHIP DARAM B0 */
B1 : origin = 300h , length = 100h /* ON CHIP DARAM B1 */
B2 : origin = 60h , length = 20h /* ON CHIP DARAM B2 */
}
/*--------------------------------------------------------------------------*/
/* SECTIONS ALLOCATION */
/*--------------------------------------------------------------------------*/
SECTIONS
{
vectors : {} > VECS PAGE 0 /* int. vectors */
.text : {} > PROGM PAGE 0 /* code */
.cinit : {} > PROGM PAGE 0 /* init. tables */
.switch : {} > PROGM PAGE 0 /* switch, case */
.const : {} > B1 PAGE 1 /* data constants */
.bss : {} > B0 PAGE 1 /* global static var. */
.sysmem : {} > B1 PAGE 1 /* c system heap */
.data : {} > B1 PAGE 1
.stack : {} > B1 PAGE 1 /* c system stack */
}
我已经调整过memory了,跳过加密区了,还是有这样的问题
报错是这样的:
Warning!The DSP is configured for microprocessor mode.To program the on-chip flash,the DSP must be configured for microcontroller mode.
If you are using an eZdsp TMS320LF2407 or eZdsp TMS320LF2407A,move jumper JP4 from location 1-2 to 2-3,if you are using a TMS320LF2407/2407A EVM,move jumper JP6 from location 1-2 to 2-3.
老提示要配置成MC模式,但我已经将MP/MC引脚接地,VCCP引脚接5V了啊
不知什么原因,请个位帮忙!
谢谢