This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 cpld 电流很大



请教

28335+cpld 电路板,焊好板子后,直接上电(28335和cpld都空片,里面没有程序),3.3V被拉低到1.4V。但是两块芯片都不发热。28335与cpld之间总线连接,16bit数据10bit地址,还有一些互联的IO口(包括pwm口),两片相连的线有60条。使用了28335内部AD,使用外部参考电压,目前该参考电压未加入。

1.9V采用ti的电源芯片,3.3V用1117-3.3。焊了3块板,都是直接上电,芯片是空片。 存在的情况,3块板的3.3V都被拉低(1.4V-1.5V)。其中1块板1.9V对GND已经短路。 请大家帮助分析下。。。着急

已经做了如下实验,只焊接28335(空片无程序)最小系统,3.3V正常。测量pwm输出为低,ad引脚为低,其他IO输出为高。

只焊接cpld(空片无程序),3.3V正常,IO引脚电平为3.3V。现在的问题是两者都焊接,上电就不行。

下步计划,先给28335内核供电,手动开关加入3.3V,割断PWM与cpld之间的连接。