#ifndef __SPEED_EST_H__
#define __SPEED_EST_H__
typedef struct {
_iq EstimatedTheta; // Input: Electrical angle (pu)
_iq OldEstimatedTheta; // History: Electrical angle at previous step (pu)
_iq EstimatedSpeed; // Output: Estimated speed in per-unit (pu)
Uint32 BaseRpm; // Parameter: Base speed in rpm (Q0) - independently with global Q
_iq21 K1; // Parameter: Constant for differentiator (Q21) - independently with global Q
_iq K2; // Parameter: Constant for low-pass filter (pu)
_iq K3; // Parameter: Constant for low-pass filter (pu)
int32 EstimatedSpeedRpm; // Output : Estimated speed in rpm (Q0) - independently with global Q
_iq Temp; // Variable : Temp variable
} SPEED_ESTIMATION; // Data type created
/*-----------------------------------------------------------------------------
Default initalizer for the SPEED_ESTIMATION object.
-----------------------------------------------------------------------------*/
#define SPEED_ESTIMATION_DEFAULTS { 0, \
0, \
0, \
0, \
0, \
0, \
0, \
0, \
0, \
}
#define SE_DIFF_MAX_LIMIT _IQ(0.85)
#define SE_DIFF_MIN_LIMIT _IQ(0.15)
/*------------------------------------------------------------------------------
SPEED_EST Macro Definition
------------------------------------------------------------------------------*/
#define SE_MACRO(v) \
if ((v.EstimatedTheta < SE_DIFF_MAX_LIMIT)&(v.EstimatedTheta > SE_DIFF_MIN_LIMIT)) \
v.Temp = _IQmpy(v.K1,(v.EstimatedTheta - v.OldEstimatedTheta)); \
/* Q21 = Q21*(GLOBAL_Q-GLOBAL_Q) */ \
else v.Temp = _IQtoIQ21(v.EstimatedSpeed); \
\
/* Low-pass filter */ \
/* Q21 = GLOBAL_Q*Q21 + GLOBAL_Q*Q21 */ \
v.Temp = _IQmpy(v.K2,_IQtoIQ21(v.EstimatedSpeed))+_IQmpy(v.K3,v.Temp); \
\
/* Saturate the output */ \
v.Temp=_IQsat(v.Temp,_IQ21(1),_IQ21(-1)); \
v.EstimatedSpeed = _IQ21toIQ(v.Temp); \
\
/* Update the electrical angle */ \
v.OldEstimatedTheta = v.EstimatedTheta; \
\
/* Change motor speed from pu value to rpm value (GLOBAL_Q -> Q0)*/ \
/* Q0 = Q0*GLOBAL_Q => _IQXmpy(), X = GLOBAL_Q*/ \
v.EstimatedSpeedRpm = _IQmpy(v.BaseRpm,v.EstimatedSpeed);
#endif // __SPEED_EST_H__