335中断中有如下描述
If interrupts are enabled, but the interrupt flag is already set, then the counter will hold its output high
until the ENTFLG[INT] flag is cleared. This allows for one interrupt to be pending while one is serviced.
就是一个中断进来,又有一个中断的话会被hold住,等待执行结束后再次执行,如果我想配置为中断执行时直接丢弃新的中断,该如何配置。
目前的应用是PWM有外部同步信号输入,中断还是用0和周期中断,中断执行时可能有同步信号输入再次产生中断,目前是想把同步信号的中断丢弃掉,如何配置寄存器