This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35最新调试问题,请专家看看



上电复位C28与M3都正常运行,C28周期1s,M3周期100ms。

仿真M3时:当开始擦写M3 FLASH准备RPOGRAM时C28停止运行,LDAD完成后开始运行M3,M3正常运行,但C28还是不运行。

仿真C28时:当开始擦写C28 FLASH准备RPOGRAM时M3周期由正常周期下的100 ms变成200ms,LDAD完成后开始运行C28,C28周期变成2s,M3周期还是200ms。

我分析:当仿真M3的时候,由于C28没有复位,所以在擦写M3 FLASH,C28停止运行后就不能正常进入BOOTROM,也就不能运行。

仿真C28的时候,擦写C28 FLASH导致了M3的主频降低了一半,所以后面运行时也导致C28的主频降低了一半。