This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:28377S的ADC差分模式下的模拟电压输入



目前在使用28377S的差分16位ADC,但在DATASHEET和MANUAL两本手册中,都没有找到差分输入的模拟信号对模拟地的最高电压是多少?最低又是多少?

假如我采集的信号是交流的,我把参考电压设置为3V,那么在进入ADC之前,我把交流信号偏置3V,交流最高值可能接近6V,是否可以?

或者我采用2.5V作为参考电压,交流信号偏置2.5V,交流最高值可能接近5V,是否可以?

谢谢。