This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本人基于TI提供的2812的关于三个例程《Example_281xAdcSeq_ovdTest》、《Example_281xAdcSeqModeTest》、《Example_281xAdcSoc》;在进行2812最小系统板测试的时候EvaRegs.T1CNT和EvbRegs.T3CNT这两个值都会在0或2989两个数据变动,不是0就是2989,不知道怎么回事了。仿真器为XDS100V3,CCS6.2,WIN8系统下。
在CCS6.2导入这些工程项目的时候发现这些工程项目原先都是基于CCS3.3的,所以在初始的时候在设置界面下就General界面下Products一栏下的XDAIS前方框选项去掉不选。
您好,
使用ccs6.2导入ccs3.3工程时,是否Project->Import exsisting CCS/Eclipse project?
编译能够通过吗?
谢谢大家集思广益了呢,我原先使用的是网上购买的TMS320F2812最小系统板,一直有关于AD的问题的,现在更换了开发板,同时也在产品控制板上进行了测试,发现都是可以正常编译、下载和调试的,这个应该是最小系统板的问题了。
最小系统板主要是管脚基本都是悬空的,另外电源来源是miniUSB,所以不知道这方面是不是会有些问题??
再补充说明一下,我的之前有问题的核心板的内核电压1.82V,可以下载程序,但不能开通关于ADC的下面两条语句,否则运行时不正常,如之前所述。
AdcRegs.ADCTRL3.bit.ADCBGRFDN = 0x3;
AdcRegs.ADCTRL3.bit.ADCPWDN = 1;
接下来自己工程师这出来的F2812的板子内核电压1.84V左右,其中有一块开始可以正常使用,后来却在下载程序的过程中报错(片上FLASH擦除和烧录的过程中)了。另外的板子以及基于硬汉电子的开发板都可以正常使用,不知道这个内核电压对程序下载过程中针对芯片FLASH的擦除、烧录等有没有影响的,其可靠性如何评估?平台和工作还是如上述所介绍的。
关于我的最小系统核心板的AD问题(内核电压1.81V),我将SysCtrlRegs.PLLCR=0x000A;改动为SysCtrlRegs.PLLCR=0x6以后可以正常的下载并调试程序了,并且AD采样所对应的结果寄存器的数值看上去也对上了,此时主频已然降到了90MHz,以此与大家共享.