This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035采用有源晶振调试问题

各位大神:

        请教下,28035在使用外部晶振情况下,配置成外部晶振可以独立运行软件(外部时钟引脚是GPIO19),但插上仿真器就不能仿真,使用开发环境为 Version: 6.1.0.00104 ; 仿真器是: XDS100V2,是仿真器和外部时钟不能同时使用吗?

配置如下:

EALLOW;

       SysCtrlRegs.CLKCTL.bit.XTALOSCOFF = 1;

       //   SysCtrlRegs.XCLK.bit.XCLKINSEL = 1;

       SysCtrlRegs.CLKCTL.bit.XCLKINOFF = 0;

       SysCtrlRegs.CLKCTL.bit.OSCCLKSRC2SEL = 0;  // Switch to external clock

       SysCtrlRegs.CLKCTL.bit.OSCCLKSRCSEL = 1;   // Switch from INTOSC1 to INTOSC2/ext clk

       SysCtrlRegs.CLKCTL.bit.WDCLKSRCSEL = 1;    // Switch Watchdog Clk Src to external clock

       SysCtrlRegs.CLKCTL.bit.INTOSC2OFF = 1;     // Turn off INTOSC2

       SysCtrlRegs.CLKCTL.bit.INTOSC1OFF = 1;     // Turn off INTOSC1

       EDIS;

 

有源晶振时钟是20M,有测试过时钟波形是正常的;

请教下28035这颗芯片支持使用有源晶振的情况下可以同时在线仿真吗?

请教下用V130底下的哪个例程可以测试外部有源时钟的在线调试?C:\ti\controlSUITE\device_support\f2803x\v130\DSP2803x_examples_ccsv5