This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问GPIO的GPBQSEL寄存器的作用?

看到在配置SPI的例程里,将GPBQSEL寄存器配置成3,查了下datasheet也没太理解,能否帮忙解释下具体有什么作用?

  • GPAQSEL2,GPBQSEL1,GPBQSEL2选择GPIO引脚的输入 限制类型,即
    1、异步输入模式:用于不需输入同步或自身具有信号同步功能的外设如SCI, SPI,eCAN。如果是GPIO,则该功能失效 2、仅与SYSCLKOUT同步:引脚复位时的默认模式 3、通过采样窗限制:先与SYSCLKOUT同步,然后经过采样窗得到信号。 (1)采样周期:用户设定,用GPxCTRL的QUALPRDn位决定 (2)采样窗长度:一个采样窗内可包含3次或6次采样,采样窗包含的采样 周期个数比采样数少1.GPAQSEL1/2和GPBQSEL1/2设置。