This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28069 can通信问题



F2806*例程back2back 适用的时钟频率是80Mhz这样can通信速率是1Mhz,但是F28069的时钟频率是90Mhz,需要怎么样才能更改使其传输速率为1M?附上代码,求大神们纠错

//###########################################################################
//
// FILE: F2806x_ECan.c
//
// TITLE: F2806x Enhanced CAN Initialization & Support Functions.
//
//###########################################################################
// $TI Release: F2806x C/C++ Header Files and Peripheral Examples V150 $
// $Release Date: June 16, 2015 $
// $Copyright: Copyright (C) 2011-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################

#include "F2806x_Device.h" // F2806x Headerfile Include File
#include "F2806x_Examples.h" // F2806x Examples Include File

//---------------------------------------------------------------------------
// InitECan:
//---------------------------------------------------------------------------
// This function initializes the eCAN module to a known state.
//
#if DSP28_ECANA
void InitECan(void)
{
InitECana();
}
#endif

#if DSP28_ECANA
void InitECana(void) // Initialize eCAN-A module
{

/* Create a shadow register structure for the CAN control registers. This is
needed, since only 32-bit access is allowed to these registers. 16-bit access
to these registers could potentially corrupt the register contents or return
false data. */

struct ECAN_REGS ECanaShadow;

EALLOW; // EALLOW enables access to protected bits

/* Configure eCAN RX and TX pins for CAN operation using eCAN regs*/

ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
ECanaShadow.CANTIOC.bit.TXFUNC = 1;
ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;

ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
ECanaShadow.CANRIOC.bit.RXFUNC = 1;
ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;

/* Configure eCAN for HECC mode - (reqd to access mailboxes 16 thru 31) */
// HECC mode also enables time-stamping feature

ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.SCB = 1;
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;

/* Initialize all bits of 'Message Control Register' to zero */
// Some bits of MSGCTRL register come up in an unknown state. For proper operation,
// all bits (including reserved bits) of MSGCTRL must be initialized to zero

ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;

// TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
// as a matter of precaution.

ECanaRegs.CANTA.all = 0xFFFFFFFF; /* Clear all TAn bits */

ECanaRegs.CANRMP.all = 0xFFFFFFFF; /* Clear all RMPn bits */

ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;

/* Configure bit timing parameters for eCANA*/

ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;

// Wait until the CPU has been granted permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..

ECanaShadow.CANBTC.all = 0;
/* The following block is for 80 MHz SYSCLKOUT. (40 MHz CAN module clock Bit rate = 1 Mbps
See Note at end of file. */

ECanaShadow.CANBTC.bit.BRPREG = 2;
ECanaShadow.CANBTC.bit.TSEG2REG = 3;
ECanaShadow.CANBTC.bit.TSEG1REG = 9;

ECanaShadow.CANBTC.bit.SAM = 1;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;

ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;

// Wait until the CPU no longer has permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..

/* Disable all Mailboxes */
ECanaRegs.CANME.all = 0; // Required before writing the MSGIDs

EDIS;
}
#endif // endif DSP28_ECANA

//---------------------------------------------------------------------------
// Example: InitECanGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as eCAN pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// Only one GPIO pin should be enabled for CANTXA operation.
// Only one GPIO pin shoudl be enabled for CANRXA operation.
// Comment out other unwanted lines.

#if DSP28_ECANA
void InitECanGpio(void)
{
InitECanaGpio();
}
#endif

#if DSP28_ECANA
void InitECanaGpio(void)
{
EALLOW;

/* Enable internal pull-up for the selected CAN pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.

GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pull-up for GPIO30 (CANRXA)
GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pull-up for GPIO31 (CANTXA)

/* Set qualification for selected CAN pins to asynch only */
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.

GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3; // Asynch qual for GPIO30 (CANRXA)

/* Configure eCAN-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAN functional pins.

GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // Configure GPIO30 for CANRXA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // Configure GPIO31 for CANTXA operation

EDIS;
}
#endif // endif DSP28_ECANA

/* Note: Bit timing parameters must be chosen based on the network parameters such as
the sampling point desired and the propagation delay of the network. The propagation
delay is a function of length of the cable, delay introduced by the
transceivers and opto/galvanic-isolators (if any).

The parameters used in this file must be changed taking into account the above mentioned
factors in order to arrive at the bit-timing parameters suitable for a network.
*/

//===========================================================================
// End of file.
//===========================================================================

  • 主程序如下:

    //###########################################################################
    // Description
    //! \addtogroup f2833x_example_list
    //! <h1>eCAN-A to eCAN-B Trasmit Loop (ecan_a_to_b_xmit)</h1>
    //!
    //! This example TRANSMITS data to another CAN module using MAILBOX5
    //! This program could either loop forever or transmit "n" # of times,
    //! where "n" is the TXCOUNT value. \n
    //!
    //! This example can be used to check CAN-A and CAN-B. Since CAN-B is
    //! initialized in DSP2833x_ECan.c, it will acknowledge all frames
    //! transmitted by the node on which this code runs. Both CAN ports of
    //! the 2833x DSP need to be connected to each other (via CAN transceivers)
    //!
    //! \b External \b Connections \n
    //! - eCANA is on GPIO31 (CANTXA) and GPIO30 (CANRXA)
    //! - eCANB is on GPIO8 (CANTXB) and GPIO10 (CANRXB)
    //! - Connect eCANA to eCANB via CAN transceivers
    //
    //###########################################################################
    // $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $
    // $Release Date: November 1, 2016 $
    // $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated -
    // http://www.ti.com/ ALL RIGHTS RESERVED $
    //###########################################################################

    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File

    #define TXCOUNT 100 // Transmission will take place (TXCOUNT) times..

    // Globals for this example
    long i;
    long loopcount = 0;
    void delay_ms(unsigned int t);
    void main()
    {
    // Create a shadow register structure for the CAN control registers. This is
    // needed, since only 32-bit access is allowed to these registers. 16-bit access
    // to these registers could potentially corrupt the register contents or return
    // false data.

    struct ECAN_REGS ECanaShadow;

    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the DSP2833x_SysCtrl.c file.
    InitSysCtrl();

    // Step 2. Initialize GPIO:
    // This example function is found in the DSP2833x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // InitGpio(); // Skipped for this example

    // Just initialize eCAN pins for this example
    // This function is in DSP2833x_ECan.c
    InitECanGpio();

    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    DINT;

    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the DSP2833x_PieCtrl.c file.
    InitPieCtrl();

    // Disable CPU interrupts and clear all CPU interrupt flags:
    IER = 0x0000;
    IFR = 0x0000;

    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example. This is useful for debug purposes.
    // The shell ISR routines are found in DSP2833x_DefaultIsr.c.
    // This function is found in DSP2833x_PieVect.c.
    InitPieVectTable();

    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.

    // No interrupts used in this example.

    // Step 4. Initialize all the Device Peripherals:
    // This function is found in DSP2833x_InitPeripherals.c
    // InitPeripherals(); // Not required for this example

    // In this case just initialize eCAN-A and eCAN-B
    // This function is in DSP2833x_ECan.c
    InitECan();

    // Step 5. User specific code:

    /* Write to the MSGID field */
    //设置接收邮箱
    //设置接收邮箱的ID,扩展帧
    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaRegs.CANME.bit.ME16= 0;
    ECanaMboxes.MBOX16.MSGID.all = 0x80C20000;//邮箱ID???怎么设置

    //设置邮箱16为接收邮箱
    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.bit.MD16 =1;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;

    //数据长度 8个BYTE
    ECanaMboxes.MBOX16.MSGCTRL.bit.DLC = 8;

    //没有远方应答帧被请求*/
    ECanaMboxes.MBOX16.MSGCTRL.bit.RTR = 0;

    //邮箱使能
    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaShadow.CANME.bit.ME16 =1;
    ECanaRegs.CANME.all = ECanaShadow.CANME.all;

    //邮箱中断使能
    EALLOW;
    ECanaRegs.CANMIM.all = 0xFFFFFFFF;
    //邮箱中断将产生在ECAN0INT
    ECanaRegs.CANMIL.all = 0;
    ECanaRegs.CANGIF0.all = 0xFFFFFFFF;
    //ECAN0INT中断请求线被使能
    ECanaRegs.CANGIM.bit.I0EN = 1;
    EDIS;
    //使能PIE中断
    PieCtrlRegs.PIEIER9.bit.INTx5 = 1;

    //使能CPU中断
    IER |= M_INT9;

    EINT; //开全局中断
    ERTM; //开实时中断
    //设置can_ID
    ECanaMboxes.MBOX25.MSGID.all = 0x110; // Extended Identifier,做标准帧,不做为扩展帧了

    /* Configure Mailbox under test as a Transmit mailbox */

    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.bit.MD25 = 0;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;

    /* Enable Mailbox under test */

    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaShadow.CANME.bit.ME25 = 1;
    ECanaRegs.CANME.all = ECanaShadow.CANME.all;
    delay_ms(500);

    //对1组驱动器进行复位

    /* Write to DLC field in Master Control reg */

    ECanaMboxes.MBOX25.MSGCTRL.bit.DLC = 8; //设置数据长度的字节数//

    /* Write to the mailbox RAM field */

    ECanaMboxes.MBOX25.MDL.all = 0x55555555; //往发送邮箱中写数据,分别写低32位4字节和高32位4字节
    ECanaMboxes.MBOX25.MDH.all = 0x55555555;

    /* Begin transmitting */
    //置位准备发送,将发送请求位置位,使能邮箱发送功能

    for(i=0; i < TXCOUNT; i++)
    {
    ECanaShadow.CANTRS.all = 0;
    ECanaShadow.CANTRS.bit.TRS25 = 1; // Set TRS for mailbox under test
    ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all;

    do
    {
    ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;
    } while(ECanaShadow.CANTA.bit.TA25 == 0 ); // Wait for TA5 bit to be set..


    ECanaShadow.CANTA.all = 0;
    ECanaShadow.CANTA.bit.TA25 = 1; // Clear TA5
    ECanaRegs.CANTA.all = ECanaShadow.CANTA.all;

    loopcount ++;
    }

    delay_ms(500);
    //设置can_ID
    ECanaMboxes.MBOX25.MSGID.all = 0x111; // Extended Identifier,做标准帧,不做为扩展帧了
    /* Write to the mailbox RAM field */

    ECanaMboxes.MBOX25.MDL.all = 0x55555555; //往发送邮箱中写数据,分别写低32位4字节和高32位4字节
    ECanaMboxes.MBOX25.MDH.all = 0x55555501;

    /* Begin transmitting */
    //置位准备发送,将发送请求位置位,使能邮箱发送功能

    for(i=0; i < TXCOUNT; i++)
    {
    ECanaShadow.CANTRS.all = 0;
    ECanaShadow.CANTRS.bit.TRS25 = 1; // Set TRS for mailbox under test
    ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all;

    do
    {
    ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;
    } while(ECanaShadow.CANTA.bit.TA25 == 0 ); // Wait for TA5 bit to be set..


    ECanaShadow.CANTA.all = 0;
    ECanaShadow.CANTA.bit.TA25 = 1; // Clear TA5
    ECanaRegs.CANTA.all = ECanaShadow.CANTA.all;

    loopcount ++;
    }

    delay_ms(500);
    ECanaMboxes.MBOX25.MSGID.all = 0x112; // Extended Identifier,做标准帧,不做为扩展帧了
    /* Write to the mailbox RAM field */

    ECanaMboxes.MBOX25.MDL.all = 0x55555555; //往发送邮箱中写数据,分别写低32位4字节和高32位4字节
    ECanaMboxes.MBOX25.MDH.all = 0x5555080D;

    /* Begin transmitting */
    //置位准备发送,将发送请求位置位,使能邮箱发送功能

    for(i=0; i < TXCOUNT; i++)
    {
    ECanaShadow.CANTRS.all = 0;
    ECanaShadow.CANTRS.bit.TRS25 = 1; // Set TRS for mailbox under test
    ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all;

    do
    {
    ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;
    } while(ECanaShadow.CANTA.bit.TA25 == 0 ); // Wait for TA5 bit to be set..


    ECanaShadow.CANTA.all = 0;
    ECanaShadow.CANTA.bit.TA25 = 1; // Clear TA5
    ECanaRegs.CANTA.all = ECanaShadow.CANTA.all;

    loopcount ++;
    }


    __asm(" ESTOP0"); // Stop here
    }

    //延时函数
    void delay_ms(unsigned int t)
    {
    unsigned int i;
    for( i=0;i<t;i++)
    {
    unsigned int a=37500; //at 168MHz 42000 is ok
    while(a--);
    }
    }

    void delay_us(unsigned int t)
    {
    unsigned int i;
    for( i=0;i<t;i++)
    {
    unsigned int a=38; //at 168MHz 40 is ok,the higher the number the more timing precise
    while(a--);
    }
    }

  • 您好,

    请参考收据手册http://www.ti.com.cn/cn/lit/ug/spruh18g/spruh18g.pdf  16.10.2章节CAN Bit Rate Calculation。