This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HRCAP问题,希望大师尽快帮我解惑!

Other Parts Discussed in Thread: TMS320F28069

我使用的器件是TMS320F28069,同时要用到USB和HRCAP外设,他们共同使用SYSCLK2时钟,我设置为60MHz,说是这个频率对USB外设最适合。HRCAP捕获外部约1KHz的PWM波,占空比1%到99%。经过计算发现用60MHz时钟,HRCAP的16bit计数器会有溢出,这样有了2个问题:

1.  如果把SYSCLK2降低到30MHz,USB能不能做到接近1.2Mbps的全速?

2. 如果保持SYSCLK2为60MHz,用HRCAP库函数Uint32 PeriodWidthFall0 (Uint16 * ptrHRCAPmodule),该函数具备不具备把16bit计数器扩展到32计数能力,我看返回值是Uint32类型。

非常感谢!

  • INTOSC1 (Internal Zero-pin Oscillator 1): This is the on-chip internal oscillator 1 and provides a 10-
    MHz clock. If used as a clock source for HRCAP, the oscillator compensation routine should be called
    frequently. Because of accuracy requirements, INTOSC1 cannot be used as a clock source for the
    USB.


    内部晶振不能用于USB时钟源吗?