大家好!
我原来用的48V的电机,用DRV8301驱动没有问题,现在需要做520V的直流电机,给DRV8301采用24V供电,用DRV8301的输出直接驱动800V的mosFET管或IPM模块,请问可以用DRV8301驱动800V的IPM模块或mosFET管吗?电机功率700W。
如果可以用,怎么选择mosFET和IPM的参数?需要注意哪些参数?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.