This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用28335的同一个ADC的不同通道测量同一个电压基准,结果不同



都不是每次采样的第一个采样值,测量一个2.5V的电压基准,确保电压基准和芯片供电电压都很平稳,没有什么噪声。

每次上电测量的偏置不同,大的能差接近40个LSB,但波动小于4个LSB。

下面是5次上电ADC测量的均值

通道4: 3406 3434 3439 3410 3442

通道6:    3420 3424 3432 3434 3421

求解。。