This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的工程师们,
小弟之前用F28335,一直使用SYS/BIOS,觉得很方便。目前买了F28377D的开发板正在学习中,目前遇到的问题是。CPU1和CPU2我都想使用,而且还都用了SYS/BIOS, 但是发现烧写后,断电也只是CPU1在运行,CPU2不工作。(在不使用SYS/BIOS时,CPU1和CPU2从Flash运行的方法,我已经会了)
我在TI相关的网站上到处查找也没找到CPU1和CPU2都使用SYS/BIOS的例子,求工程师大神赐我一个,万分感谢!
我目前怀疑是TMS320F28377D.cmd文件在CPU1和CPU2的工程里需要修改一下。但是尝试了很多次也没有解决问题!
如果CPU2不能使用SYS/BIOS,那我想知道一下原因。如果CPU2可以,强烈建议TI官方SYS/BIOS的资料的例程里对F2837xD系列弄一个CPU1和CPU2都同时运行SYS/BIOS的例子!
我坚持每天自己顶帖!