源代码没有改动,怎么就错误了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
**** Build of configuration F2802x_FLASH for project HVPSFB_VMC ****
"D:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../HVPSFB-DPL-ISR.asm'
'Invoking: C2000 Compiler'
"D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/bin/cl2000" -v28 -ml -mt --include_path="Q:/TI/development_kits/HVPSFB_v1.1/HVPSFB_VMC" --include_path="D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/asm" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_headers/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/include" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_common/include" --include_path="Q:/TI/development_kits/~SupportFiles/F2802x_headers" --include_path="Q:/TI/libs/math/IQmath/v15c/include" -g --define="_DEBUG" --define="FLASH" --define="LARGE_MODEL" --diag_warning=225 --preproc_with_compile --preproc_dependency="HVPSFB-DPL-ISR.d" "../HVPSFB-DPL-ISR.asm"
18 Assembly Errors, 1 Assembly Warning
>> Compilation failure
subdir_rules.mk:42: recipe for target 'HVPSFB-DPL-ISR.obj' failed
gmake: *** No rule to make target 'Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/C/ADC_SOC_Cnf.c', needed by 'ADC_SOC_Cnf.obj'.
gmake: *** No rule to make target 'Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/C/DAC_Cnf.c', needed by 'DAC_Cnf.obj'.
gmake: *** No rule to make target 'Q:/TI/device_support/f2802x/v129/DSP2802x_common/source/DSP2802x_CodeStartBranch.asm', needed by 'DSP2802x_CodeStartBranch.obj'.
gmake: *** No rule to make target 'Q:/TI/device_support/f2802x/v129/DSP2802x_headers/source/DSP2802x_GlobalVariableDefs.c', needed by 'DSP2802x_GlobalVariableDefs.obj'.
gmake: *** No rule to make target 'Q:/TI/device_support/f2802x/v129/DSP2802x_common/source/DSP2802x_usDelay.asm', needed by 'DSP2802x_usDelay.obj'.
"../HVPSFB-DPL-ISR.asm", line 24: fatal error: cannot open source file "PeripheralHeaderIncludes.h"
Compilation terminated.
"../HVPSFB-DPL-ISR.asm", WARNING! at line 24: [E1000] error while processing C
code in .cdecls directive
.cdecls C,NOLIST, "PeripheralHeaderIncludes.h"
"../HVPSFB-DPL-ISR.asm", ERROR! at line 26: [E1000] Include/Copy file not
found or opened
.include "ADCDRV_4ch.asm"
"../HVPSFB-DPL-ISR.asm", ERROR! at line 27: [E1000] Include/Copy file not
found or opened
.include "PWMDRV_PSFB_VMC_SR.asm"
"../HVPSFB-DPL-ISR.asm", ERROR! at line 28: [E1000] Include/Copy file not
found or opened
.include "CNTL_2P2Z.asm"
"../HVPSFB-DPL-ISR.asm", ERROR! at line 77: [E0002] Invalid mnemonic
specification
ADCDRV_4CH_INIT 1,2,3,4
"../HVPSFB-DPL-ISR.asm", ERROR! at line 78: [E0002] Invalid mnemonic
specification
PWMDRV_PSFB_VMC_SR_INIT 1,2,4 ; ePWMs 1,2 and 4
"../HVPSFB-DPL-ISR.asm", ERROR! at line 117: [E0002] Invalid mnemonic
specification
ADCDRV_4ch 1,2,3,4 ; Read ADC results
"../HVPSFB-DPL-ISR.asm", ERROR! at line 119: [E0002] Invalid mnemonic
specification
PWMDRV_PSFB_VMC_SR 1,2,4 ; Run the PWM driver
"../HVPSFB-DPL-ISR.asm", ERROR! at line 122: [E0009] Missing struct/union
member or tag
MOVW DP,#_EPwm2Regs.TBPHS
"../HVPSFB-DPL-ISR.asm", ERROR! at line 123: [E0009] Missing struct/union
member or tag
MOV AL,@_EPwm2Regs.TBPHS.half.TBPHS
"../HVPSFB-DPL-ISR.asm", ERROR! at line 123: [E0000] Expecting operand
delimiter
MOV AL,@_EPwm2Regs.TBPHS.half.TBPHS
"../HVPSFB-DPL-ISR.asm", ERROR! at line 123: [E0003] Syntax error - Operand 4
MOV AL,@_EPwm2Regs.TBPHS.half.TBPHS
"../HVPSFB-DPL-ISR.asm", ERROR! at line 124: [E0009] Missing struct/union
member or tag
ADD AL,@_EPwm2Regs.TBPRD
"../HVPSFB-DPL-ISR.asm", ERROR! at line 126: [E0009] Missing struct/union
member or tag
MOV @_EPwm2Regs.CMPB, AL ; CMPB2 = (TBPRD2 + TBPHS2)/2
"../HVPSFB-DPL-ISR.asm", ERROR! at line 165: [E0009] Missing struct/union
member or tag
MOVW DP,#_EPwm1Regs.ETCLR
"../HVPSFB-DPL-ISR.asm", ERROR! at line 166: [E0009] Missing struct/union
member or tag
MOV @_EPwm1Regs.ETCLR,#0x01 ; Clear EPWM1 Int flag
"../HVPSFB-DPL-ISR.asm", ERROR! at line 194: [E0009] Missing struct/union
member or tag
MOVW DP,#_PieCtrlRegs.PIEACK ; Acknowledge PIE interrupt Group 3
"../HVPSFB-DPL-ISR.asm", ERROR! at line 195: [E0009] Missing struct/union
member or tag
MOV @_PieCtrlRegs.PIEACK, #0x4
"../HVPSFB-DPL-ISR.asm", ERROR! at EOF: [E0300] The following symbols are
undefined:
TBPHS
CMPB
PIEACK
ETCLR
_PieCtrlRegs
_EPwm1Regs
_EPwm2Regs
TBPRD
Errors in Source - Assembler Aborted
gmake: *** [HVPSFB-DPL-ISR.obj] Error 1
'Building file: ../HVPSFB-DevInit_F2802x.c'
'Invoking: C2000 Compiler'
"D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/bin/cl2000" -v28 -ml -mt --include_path="Q:/TI/development_kits/HVPSFB_v1.1/HVPSFB_VMC" --include_path="D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/asm" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_headers/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/include" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_common/include" --include_path="Q:/TI/development_kits/~SupportFiles/F2802x_headers" --include_path="Q:/TI/libs/math/IQmath/v15c/include" -g --define="_DEBUG" --define="FLASH" --define="LARGE_MODEL" --diag_warning=225 --preproc_with_compile --preproc_dependency="HVPSFB-DevInit_F2802x.d" "../HVPSFB-DevInit_F2802x.c"
>> Compilation failure
subdir_rules.mk:49: recipe for target 'HVPSFB-DevInit_F2802x.obj' failed
"../HVPSFB-DevInit_F2802x.c", line 14: fatal error: cannot open source file "PeripheralHeaderIncludes.h"
1 catastrophic error detected in the compilation of "../HVPSFB-DevInit_F2802x.c".
Compilation terminated.
gmake: *** [HVPSFB-DevInit_F2802x.obj] Error 1
'Building file: ../HVPSFB-Main.c'
'Invoking: C2000 Compiler'
"D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/bin/cl2000" -v28 -ml -mt --include_path="Q:/TI/development_kits/HVPSFB_v1.1/HVPSFB_VMC" --include_path="D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/asm" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_headers/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/include" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_common/include" --include_path="Q:/TI/development_kits/~SupportFiles/F2802x_headers" --include_path="Q:/TI/libs/math/IQmath/v15c/include" -g --define="_DEBUG" --define="FLASH" --define="LARGE_MODEL" --diag_warning=225 --preproc_with_compile --preproc_dependency="HVPSFB-Main.d" "../HVPSFB-Main.c"
>> Compilation failure
subdir_rules.mk:56: recipe for target 'HVPSFB-Main.obj' failed
"../HVPSFB-Main.c", line 49: fatal error: cannot open source file "PeripheralHeaderIncludes.h"
1 catastrophic error detected in the compilation of "../HVPSFB-Main.c".
Compilation terminated.
gmake: *** [HVPSFB-Main.obj] Error 1
gmake: *** No rule to make target 'Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/C/PWM_PSFB_VMC_SR_Cnf.c', needed by 'PWM_PSFB_VMC_SR_Cnf.obj'.
'Building file: ../SciCommsGui.c'
'Invoking: C2000 Compiler'
"D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/bin/cl2000" -v28 -ml -mt --include_path="Q:/TI/development_kits/HVPSFB_v1.1/HVPSFB_VMC" --include_path="D:/ti/ccsv6/tools/compiler/c2000_15.12.3.LTS/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/asm" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_headers/include" --include_path="Q:/TI/libs/app_libs/digital_power/f2802x_v3.2/include" --include_path="Q:/TI/device_support/f2802x/v129/DSP2802x_common/include" --include_path="Q:/TI/development_kits/~SupportFiles/F2802x_headers" --include_path="Q:/TI/libs/math/IQmath/v15c/include" -g --define="_DEBUG" --define="FLASH" --define="LARGE_MODEL" --diag_warning=225 --preproc_with_compile --preproc_dependency="SciCommsGui.d" "../SciCommsGui.c"
>> Compilation failure
subdir_rules.mk:70: recipe for target 'SciCommsGui.obj' failed
"../SciCommsGui.c", line 11: fatal error: cannot open source file "PeripheralHeaderIncludes.h"
1 catastrophic error detected in the compilation of "../SciCommsGui.c".
Compilation terminated.
gmake: *** [SciCommsGui.obj] Error 1
gmake: *** No rule to make target 'Q:/TI/device_support/f2802x/v129/DSP2802x_headers/cmd/DSP2802x_Headers_nonBIOS.cmd', needed by 'Project_Name.out'.
gmake: *** No rule to make target 'Q:/TI/libs/math/IQmath/v15c/lib/IQmath.lib', needed by 'Project_Name.out'.
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
应该是你工程路径的问题,我编译了可以通过,先检查下路径是否都对!