This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2806 EPWM不同步



应用EPWM1和EPWM2产生相同的波形,但是示波器测量他们不同步,相差2个时钟周期?

  • 程序是怎么写的?设置Time Base同步了没有

  • EPwm1Regs.TBPRD = 500; // Period = 500 TBCLK counts

    EPwm1Regs.TBPHS.half.TBPHS = 0; // Set Phase register to zero

    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Asymmetrical mode

    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Master module

    EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;

    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1 ;

    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module

    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;

    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

    EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // set actions for EPWM1A

    EPwm1Regs.AQCTLA.bit.PRD = AQ_CLEAR;

    EPwm2Regs.TBPRD = 500; // Period = 500 TBCLK counts

    EPwm2Regs.TBPHS.half.TBPHS = 0; // Set Phase register to zero

    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Asymmetrical mode

    EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Master module

    EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;

    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1 ;

    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Sync down-stream module

    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;

    EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

    EPwm2Regs.AQCTLA.bit.ZRO = AQ_SET; // set actions for EPWM1A

    EPwm2Regs.AQCTLA.bit.PRD = AQ_CLEAR;

  • 看CCS中,EPwm1Regs.TBCTR和EPwm2Regs.TBCTR总是相差2?什么原因,等待解答!

  • 谁来解答呢?

  • 楼主你好,

    设置同步以后,主同步ePWM模块和其他被同步的ePWM单元间会有计数值差,其它被同步的单元之间计数值是一样的。

    这一点规格书里有详细描述如下:

    EPWMxSYNCI: Synchronization Input Pulse:

    The value of the phase register is loaded into the counter register when an input synchronization pulse

    is detected (TBPHS ® TBCTR). This operation occurs on the next valid time-base clock (TBCLK)

    edge.

    The delay from internal master module to slave modules is given by:

    – if ( TBCLK = SYSCLKOUT): 2 x SYSCLKOUT

    – if ( TBCLK != SYSCLKOUT):1 TBCLK